cancel
Showing results for 
Search instead for 
Did you mean: 

USBX CDC ACM on STM32F407ZGT6: COM Port Recognized but Can't Connect, cdc_acm_parameterInstance Not Activated

bazhiyu
Visitor

Hi everyone,

I am trying to get a USBX CDC ACM device running on an STM32F407ZGT6, using a project generated by STM32CubeMX. I'm basing my work on the example provided for the STM32F469 (DEVICE_CDC_ACM).

Problem Description

The device is partially working. When I plug it in, Windows Device Manager recognizes it and assigns a COM port. However, when I try to connect using any terminal software (Tera Term, PuTTY, etc.), the connection fails. The software cannot open the port.

Debugging Findings

Through debugging, I've identified a key issue in the initialization sequence:

  1. Instance Activator Not Called:​ The callback function I set for cdc_acm_parameter.ux_slave_class_cdc_acm_instance_activate(which is CDC_Init_FS) is never triggered. This prevents the proper initialization of my CDC ACM instance.

  2. Null Pointer in Thread:​ The usbx_cdc_acm_read_thread_entryfails because it encounters a null pointer. Specifically, the comparison ux_utility_memory_compare(data_interface->ux_slave_interface_class->ux_slave_class_name, ...)fails because data_interface->ux_slave_interface_classis a null pointer.

  3. Root Cause Hypothesis:​ This strongly suggests that the data interface for the CDC ACM class was not correctly associated with a class instance during the enumeration process. The ux_slave_interface_classpointer for the data interface is not being set, which is likely why the instance activator is never called.

My Setup and Configuration

  • MCU:​ STM32F407ZGT6

  • Software Packages:​ STM32CubeMX-generated code with USBX and ThreadX.

  • Reference Example:​ ST's DEVICE_CDC_ACMexample for STM32F469, which I have adapted for the F407.

What I've Already Checked/Tried

  • Clock Configuration:​ The USB clock is confirmed to be exactly 48 MHz .

  • Pin Configuration:​ The USB DP (PA12) and DM (PA11) pins are correctly configured for their alternate function.

  • Interrupts:​ The USB global interrupt is enabled in the NVIC.

  • Device Manager Recognition:​ The fact that a COM port appears indicates that the basic device descriptor is correct and the host identifies it as a CDC device at a high level .

Specific Questions

Based on the symptoms and the null pointer, I suspect the issue lies in the USB configuration descriptors or how the CDC ACM class is registered. Could you please help me with the following?

  1. What are the common reasons for the ux_slave_interface_classpointer of a data interface remaining null in a USBX CDC ACM setup?

  2. When migrating the CDC ACM example from an F469 to an F407, are there any critical changes needed in the device or configuration descriptors that are often overlooked? Specifically, should I pay special attention to the Union Functional Descriptor​ that links the control and data interfaces?

  3. In the ux_device_class_cdc_acm_activatefunction within USBX, what are the precise conditions that must be met for the instance_activatecallback to be called? My function is not being called, so one of these conditions is likely not met.

Any guidance or suggestions on where to look in the descriptor or initialization code would be greatly appreciated. Thank you for your time and expertise.

2 REPLIES 2
FBL
ST Employee

Hello @bazhiyu & welcome to ST Community

Are you using a reference board (nucleo eval or disco) as reference design? 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL
I purchased a finished STM32 development board. I have tested the USB Device middleware configured via CubeMX, and it is able to establish a connection successfully.
 
Currently, it seems that the CDC_Init_FS function is executable (meaning the breakpoint is not hit, yet the parameters have indeed deviated from their default values). However, a normal connection with the corresponding COM port still cannot be established.