2026-01-12 6:49 AM
I am using a UX_Device_Audio2.0-based project on H7.
Could this be a codec configuration issue (mixer/settings), a USB audio packet scheduling problem, or something else? I can't seem to find a fix yet.
2026-01-12 6:53 AM
> Could this be a codec configuration issue (mixer/settings), a USB audio packet scheduling problem, or something else?
Yes, yes, and yes.
Hard to guess without any info - except that it doesn't work.
2026-01-12 7:06 AM
LOL - that's funny, thanks for the laugh.
This can be tested with base example from STM32 - I just tested it on H753i-eval board.
2026-01-12 7:58 AM
... which surely everybody has and uses it that way?
;)
At least we have one more info now.
2026-01-12 9:08 AM
>This can be tested
- dont have this board.
- what sample rate you set ? Try 48k. (USB /UAC1 only working correct at 48k...afaik. Maybe UAC2 can do more...but i never tried, lost interest /too much to learn and check and program then )
- what you set/tried at host side ? + host is...Win/mixer , Linux/Alsa , pulse.., pipe ..or ?