Question
USB Host Firmware and STM32 - Pay or Free
Posted on July 11, 2012 at 15:39
Hello ALL
We have already completed a project with the STM32F It took some time to get up to speed but eventually we did, and completed a complex project. Now we have a project which could work with a similar sized STM32 but with the exception that we need to be able to plug a USB memory stick into the device and have the device save readings onto the USB stick. So now we need an STM32 with a USB host (Im assuming USB OTG wont do as Ive never seen a USB memory stick with an OTG connector) I can see the STM32F107 for the hardware, but it looks like we need to pay for a USB host stack. Is this correct or is there a freeware stack that works? If we have to pay what sort of money are we talking about? Many thanks for any assistance. Denis Many thanks for any help in advance Denis