2011-01-18 2:08 AM
USB connection
2011-05-17 5:21 AM
> i see that it is possiable to connect the USB with external PHY and without.
What is the target MCU? There are a couple of variations of external PHY (or transceiver) a) External USB transceiver for isolation - PIC18F/24F/32, etc An isolator is inserted between the MCU and the transceiver b) OTG transceiver - NXP LPC family OTG transceiver does OTG-specific protocol on the bus (SRP, HNP) These MCUs work as an embedded host or device without OTG transceiver c) UTMI/ULPI for high-speed - OMAP etc. Tsuneo2011-05-17 5:21 AM
2011-05-17 5:21 AM
> i am using the stm32f207zg.
Are you talking on this figure on the STM32F205xx/207xx datasheet?
http://www.st.com/internet/com/TECHNICAL_RESOURCES/TECHNICAL_LITERATURE/DATASHEET/CD00237391.pdf
Figure 81. OTG HS connection dual-role with external PHY
It's a ULPI PHY for high-speed OTG.
STM32F2xx has on-chip high-speed USB host and device engine. They work as just an embedded host or just an device, but not for OTG without the external ULPI PHY.
Tsuneo
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.