2013-07-23 8:56 AM
Hi there,
I'm getting started with USB. So I downloaded the STM32_USB-FS-Device_Lib_V4.0.0 and played around with the examples. I already used the Virtual COM port sucessfully on the discovery board and also included the functionality in my own project with an STM32F373. Everything fine here. Now I wanted to start using the audio class. I looked at the Audio_Speaker example project and tailored it to my hardware. It is correctly recognized as a speaker - but I get error messages on the PC when I try to play something. I already found out that no ''High priority'' interrupts occur. After the first talk to the PC there are only ''SOF''-interrupts... Can anyone give me hints? The best way to help me would be give me any audio example code (e.g. the Audio_Speaker example?) that is working on the Discovery F3 board. If I have working code I can search for the parts I missed myself. I only need the USB part, outputting the data to the DAC is then no problem any more. I could also make a project with all changes I think are necessary, if someone would like inspect it. (My current project already has several changes making it probably harder to think into for others) Kind regards, Kajetan #audio-usb-discovery-f3