cancel
Showing results for 
Search instead for 
Did you mean: 

USART2 COMMUNICATION DATA IS NOT GETTING IN SERIAL TERMINAL CALLED PUTTY

mani s
Associate III
Posted on July 13, 2018 at 08:02

I cannot any thing on serial terminal (PUTTY) ,here i'm using usart2 communication.I posted code below please let me know anything wrong in the code.

#include 'stm32f7xx.h' // Device header

#include<stdint.h>

#include <string.h>

#include <stdio.h>

int rec_data();

void send_data(char s);

void delay();

void flash_led();

void PutString( uint8_t * str);

int main()

{

// int a, n;

// float b;

LED_Initialize();

//flash_led();

//usart_snd_str('\n\rHello, please type something\n\r');

//reset clock reg

RCC -> AHB1ENR |= RCC_AHB1ENR_GPIODEN;

//reset and clock control reg ,select USART2 for APB1, pin no 18

RCC -> APB1ENR =RCC_APB1ENR_USART2EN;

// mode pd8- tx and pd9 - rx

GPIOA -> MODER &= ~(GPIO_MODER_MODER1_0);

GPIOA -> MODER |= GPIO_MODER_MODER1_1;

//alternate function A7

// GPIOA->AFR[0] |= 0x77 << (4*5);

//type of gpio alternate function

GPIOA -> OTYPER &= ~(GPIO_OTYPER_OT_2);

GPIOA -> OTYPER &= ~(GPIO_OTYPER_OT_3);

//speed

GPIOA -> OSPEEDR |= GPIO_OSPEEDER_OSPEEDR1;

//push pull resisitor

GPIOA -> PUPDR &= ~(GPIO_PUPDR_PUPDR1);

//uart_configration();

// start bit

//data word length 7 , 8 and 9

//stop 2 nd 1

//baud rate 9600

//parity bits

//mode

USART2 -> CR1 &= ~USART_CR1_M0;

USART2 -> BRR = 9600;

USART2 -> CR2 &= ~(USART_CR2_STOP_1);

USART2 -> CR1 &= ~(USART_CR1_OVER8);

USART2 -> CR1 |= (USART_CR1_TE | USART_CR1_RE );

USART2 -> CR1 |= USART_CR1_UE;

uint8_t a= 12;

PutString(&a);

}

void PutChar(int8_t ch)

{

while(!(USART2->ISR & USART_ISR_TXE));

USART2->TDR = ch;

}

void PutString( uint8_t * str)

{

while(*str != 0)

{

PutChar( *str);

str++;

}

}

int rec_data()

{

/* Wait until the data is ready to be received. */

while (!(USART2->ISR & USART_ISR_RXNE));

// read RX data, combine with DR mask (we only accept a max of 9 Bits)

return ((uint8_t)(USART2->RDR & 0xFF));

}
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0