Question
USART System Bootloader - STM32L151xx
Posted on June 08, 2015 at 22:05
Hello,
I'm trying to use the default bootloader of this STM32L151CCT6 over USART1.I've read and follow all the tips and tutorials of AN2606 and AN3155, but without sucess.This is my process to try a communication:Turn on my board
Set the microcontroller in reset mode (LOW in Reset Pin)
Set the pin BOOT0 in HIGH
Release the Reset Pin
Send 0x7F;
Wait for 0x79;
When I send 0x7F and wait for 0x79, it never returns.
Am I missing something in this process?Many thanks for any help or guidance that can be offered!