cancel
Showing results for 
Search instead for 
Did you mean: 

Up to which altitude does the STM32 work properly?

Daniel H
Associate
Posted on February 14, 2018 at 08:35

I want to shoot it in about 20km altitude, but I have doubts about if the microcontroller still works under that low pressure. Does also anyone know the distance of the conducting paths?

#altitude
This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Posted on February 15, 2018 at 08:01

to avoid issues with radiation, short tracks on the pcb, ...

Radiation is mostly about internal MCU / semiconductor problems.

With small enough structural sizes, each alpha particle hit will distort internal states, i.e. flip RAM cell contents.

That means, albeit not physically damaged, it will do weird things up there.