cancel
Showing results for 
Search instead for 
Did you mean: 

Hello-World for CAN-Communication (with minimal setup) on Nucleo-f091rc

ajaygargnsit
Associate II
Posted on February 13, 2018 at 08:34

Hi All.

We have been trying to set up CAN-communication, and have been unsuccessful so far.

So, we are wishing to proceed in baby-steps.

As a first step, we intend to get the sending-CAN-packet working.

Firstly, is it possible to get it working with just one node on the CAN-bus?

Right now, with one board + one controller + one transceiver + one level-shifter,  we receive timeout while doing HAL_CAN_Transmit.

I can present more details, but I would be grateful for an answer to the following question first ::

Is it possible to have HAL_CAN_Transmit working without any timeout,  with just one node (the transmitting node itself) on the CAN-bus?

 

Thanks and Regards,

Ajay

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
T J
Lead
Posted on February 13, 2018 at 08:45

Hi, Yes, you can have one node on a canbus network.

Generally Nodes only transmit their data, so its quite normal for the node to transmit only.

However,

it is much better for you, to buy a known good transmitter, like CanDo, and set it up to send frames every 10mS,

then you should work on the receiver first.

I have the CanBus systems running on my '091 and '767 boards.

I used the cube and the CanDo unit to start.

if you don't have a canbus line driver connected, the board will hang, you need a pullup on the Rx pin.

Rule: no two units should be able to transmit the same message ID.

set ABOM true.

View solution in original post

7 REPLIES 7
T J
Lead
Posted on February 13, 2018 at 08:45

Hi, Yes, you can have one node on a canbus network.

Generally Nodes only transmit their data, so its quite normal for the node to transmit only.

However,

it is much better for you, to buy a known good transmitter, like CanDo, and set it up to send frames every 10mS,

then you should work on the receiver first.

I have the CanBus systems running on my '091 and '767 boards.

I used the cube and the CanDo unit to start.

if you don't have a canbus line driver connected, the board will hang, you need a pullup on the Rx pin.

Rule: no two units should be able to transmit the same message ID.

set ABOM true.

ajaygargnsit
Associate II
Posted on February 13, 2018 at 10:09

Thanks T J.

You have arrived as our Saviour !!

Setting ABOM to ENABLE, we have made a great deal of progress.

Earlier, when ABOM was DISABLE, we were seeing absolutely nothing on the controller/transceiver pins when sending the CAN-packet.

Now, with ABOM set to ENABLE, we see the waveform on the controller as well the transceiver pin upon sending the CAN-packet.

So, courtesy you, we have been able to move forward after 36 hours of slogging.

However, HAL_CAN_Transmit (with 5-seconds timeout argument) still results in HAL_TIMEOUT.

What could be the possible issue for this?

Following are the two init-functions being used ::

###############################################################

void MX_CAN_Init(void)

  hcan.Instance = CAN;

  hcan.Init.Prescaler = 16;

  hcan.Init.Mode = CAN_MODE_NORMAL;

  hcan.Init.SJW = CAN_SJW_1TQ;

  hcan.Init.BS1 = CAN_BS1_1TQ;

  hcan.Init.BS2 = CAN_BS2_1TQ;

  hcan.Init.TTCM = DISABLE;

  hcan.Init.ABOM = ENABLE;

  hcan.Init.AWUM = DISABLE;

  hcan.Init.NART = DISABLE;

  hcan.Init.RFLM = DISABLE;

  hcan.Init.TXFP = DISABLE;

  if (HAL_CAN_Init(&hcan) != HAL_OK)

  {

    _Error_Handler(__FILE__, __LINE__);

  } 

}

 

void HAL_CAN_MspInit(CAN_HandleTypeDef* canHandle)

  GPIO_InitTypeDef GPIO_InitStruct;

  if(canHandle->Instance==CAN)

  {

    __HAL_RCC_CAN1_CLK_ENABLE();

   

    /* PA11     ------> CAN_RX, PA12     ------> CAN_TX  */

    GPIO_InitStruct.Pin = GPIO_PIN_11| GPIO_PIN_12;

    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;

    GPIO_InitStruct.Pull = GPIO_NOPULL;

    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;

    GPIO_InitStruct.Alternate = GPIO_AF4_CAN;

    HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

  }

}

########################################################################

Once again, thanks a ton for the quick reply, and you have re-instilled hope in us

Will be grateful to listen more from you.

Thanks and Regards,

Ajay

Posted on February 13, 2018 at 13:25

The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6uU&d=%2Fa%2F0X0000000bxo%2F7VRNDwgTY00gXdaVr4uG9bL5eoRb5QU5PYrIPZe41h8&asPdf=false
Posted on February 14, 2018 at 07:02

Hi T J.

Thanks for the reply.

So, if I understand correctly,

* HAL_CAN_Transmit cannot be used, it will always result in timeout, right?

* HAL_CAN_Trasnmit_IT has to be used, which need relying on interrupts (even for a purely transmitting-mode), right?

Now, we are unable to obtain ANY interrupts, even after enabling CEC/CAN interrupt-handler.

Absolutely nothing is being observed in CEC_CAN_IRQHandler

Anyhow, it looks very counter-intuitive, for interrupts to be required even for pure transmitting-mode.

It kind of defeats the purpose of HAL_CAN_Transmit method completely.

Thanks again T J.

Posted on February 14, 2018 at 07:47

Hi T J.

The CEC_CAN_IRQHandler is being hit now (earlier there were some eclipse-breakpoints issue; sorry for the noise).

Now, after calling HAL_CAN_Trasnmit_IT, the CEC_CAN_IRQHandler is hit once (as expected), but we get the following (ORed) errors ::

HAL_CAN_ERROR_EWG

HAL_CAN_ERROR_EPV

HAL_CAN_ERROR_BOF

HAL_CAN_ERROR_BD

As a result, transmission-complete is not being marked.

What can be done at hardware/software to not have these errors. and mark the transmission as successful?

Once again, thanks for your quick replies and help.

Thanks and Regards,

Ajay

Posted on February 15, 2018 at 02:42

Hi, are you still using just one unit on the canbus ?

do you have a line driver ?

is it terminated with at least 1 resistor 120R ?

Then everything worked, I actually didn't enable all those interrupts.

HAL_CAN_ERROR_EWG

HAL_CAN_ERROR_EPV

HAL_CAN_ERROR_BOF

HAL_CAN_ERROR_BD

Posted on February 15, 2018 at 07:50

Hi T J.

Now, CAN-packet sending is working.

We setup a board as the receiving-node. This board has Linux-Kernel with Flexcan1-controller enabled. And we use SocketCAN APIs to receive CAN-frames.

With the above (correctly working) receiving-node set up, HAL_CAN_Transmit (synchronous version only) returned success, and the packet was successfully received at the receiving-node.

If this receiving-node is not set up, we get HAL_TIMEOUT in HAL_CAN_Transmit as usual on the transmitting-node.

T J,

We are really grateful for your sincere, quick, to-the-point help.

Thanksss a tonnnnn !!!

Thanks and Regards,

Ajay