cancel
Showing results for 
Search instead for 
Did you mean: 

Ununsed ADC channel convert data

saimaddy123
Associate II
Posted on April 06, 2011 at 08:07

Ununsed ADC channel convert data

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
donald2
Associate II
Posted on May 17, 2011 at 14:30

The way the converter works is by taking a sample from a pin onto an internal capacitor.  During the conversion the charge on the capacitor is changed a bit in a way that looks random but is related to the bit values of the result. Even with that bumping around, the capacitor ends up with a similar voltage to what it started out with.

When the sample capacitor is then switched to a unconnected pin, the charge equalizes and again remains a noisy approximation of the same level.

It's important to keep this behavior in mind.  If you are getting a very noisy conversion, check that you are actually using the value from the channel you expect.