cancel
Showing results for 
Search instead for 
Did you mean: 

Undershoot tolerance at STM32F767IIT6

Tomas Bengtsson
Associate
Posted on May 15, 2018 at 15:10

  1. Does STM32F767IIT6 tolerate an undershoot of -0.8V lasting for 2ns at a 5V tolerant I/O?
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
T J
Lead
Posted on May 15, 2018 at 15:55

maybe, only because the 2nS is not enough time to overheat anything.

You could divert that energy by using a schottky diode from ground on that pin, clamping to -0.4v max

Imen.D
ST Employee
Posted on May 15, 2018 at 15:57

Hello

tomas.bengtsson@prevas.se

,

For the Input voltage on FT pins:VSS − 0.3V ; with maximum:VDD+4.0V

For more details, please check therelated

http://www.st.com/content/ccc/resource/technical/document/datasheet/group3/c5/37/9c/1d/a6/09/4e/1a/DM00273119/files/DM00273pdf/jcr:content/translations/en.DM00273pdf

,in the Table Voltage characteristics

Noted that V

IN

maximum value must always be respected. You should refer to Table 16 for the values of the maximum allowed injected current.

Best Regards,

Imen.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on May 15, 2018 at 16:07

maybe, only because the 2nS is not enough time to overheat anything.

This depends on the actual circuitry 'behind the pin', I would be cautious.

MOSFETs, for example, have a dV/dt limit. Exceeding that limit will kill it, without much energy involved (relative to it's total admissible power dissipation). I've seen FETs dying that way.