cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to read stm32f407 adc dma

kudiarasum
Associate II
Posted on June 29, 2015 at 19:04

Hi,

I

am tyring to read 3 adc channel through DMA

using

STM32F4 discovery board ,ADC channel 10,11,12 through  PC0,PC1,PC2 . i have connected 3 volt dc to  the all three channel, but the control seems to be failed to exit from the loop

while ((DMA_GetFlagStatus(DMA2_Stream4,DMA_FLAG_TCIF4)) != RESET) ;

please find my piece of code below

 

/* Define ADC init structures */

 

#include ''stdio.h''

 

#include ''stm32f4xx_adc.h''

 

#include ''stm32f4xx_rcc.h''

 

#include ''stm32f4xx_dma.h''

 

#include ''stm32f4xx_tim.h''

 

#include ''stm32f4xx_gpio.h''

 

#include ''misc.h''

 

#include ''app.h''

 

#define ADC_INTERNAL_REFERENCE    3300

 

#define ADC_12BIT_RES_COUNT 4096

 

#define MAX_ADC_CHANNELS    3

 

 

 

volatile unsigned int  ADCConvertedValues[MAX_ADC_CHANNELS];

 

 

 

unsigned short  ADC1_Conversion(unsigned char index)

 

{

 

        unsigned short ADCConvertedVoltage = 0;

 

        unsigned short result_adc_count = 0;

 

        while ((DMA_GetFlagStatus(DMA2_Stream4,DMA_FLAG_TCIF4)) != RESET) ;

 

        /* Clear DMA TC flag */

 

        DMA_ClearFlag(DMA2_Stream4,DMA_FLAG_TCIF4);

 

        /* Compute the voltage */

 

        result_adc_count = ADCConvertedValues[index];

 

        printf(''result_adc_count:%d\r\n'',result_adc_count);

 

        ADCConvertedVoltage = (result_adc_count * ADC_INTERNAL_REFERENCE) / ADC_12BIT_RES_COUNT;

 

        return ADCConvertedVoltage;

 

}

 

 

 

 

 

 

 

void adc_dma_init(void){

 

 

 

 GPIO_InitTypeDef      GPIO_InitStructure;

 

 ADC_InitTypeDef       ADC_InitStructure;

 

 ADC_CommonInitTypeDef ADC_CommonInitStructure;

 

 DMA_InitTypeDef       DMA_InitStructure;

 

 

 

 GPIO_StructInit(&GPIO_InitStructure);

 

 ADC_StructInit(&ADC_InitStructure);

 

 ADC_CommonStructInit(&ADC_CommonInitStructure);

 

 DMA_StructInit(&DMA_InitStructure);

 

 

 

 

 

 /**

 

   Set up the clocks are needed for the ADC

 

 */

 

 RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);

 

 RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);

 

 RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2,ENABLE);

 

 /**

 

   Initialization of the GPIO Pins [OK]

 

 */

 

 

 

 /* Analog channel configuration : PC.01, 02*/

 

 GPIO_InitStructure.GPIO_Pin   = GPIO_Pin_0 | GPIO_Pin_1| GPIO_Pin_2;

 

 GPIO_InitStructure.GPIO_Mode  = GPIO_Mode_AN;

 

 GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

 

 GPIO_Init(GPIOC, &GPIO_InitStructure);

 

 

 

 /**

 

   Config the ADC1

 

 */

 

 ADC_DeInit();

 

 ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;

 

 ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;

 

 ADC_InitStructure.ADC_ContinuousConvMode = ENABLE; //continuous conversion

 

 ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None; // NONE !Edge!

 

 ADC_InitStructure.ADC_NbrOfConversion = MAX_ADC_CHANNELS;

 

 ADC_InitStructure.ADC_ScanConvMode = ENABLE; // 1=scan more that one channel in group

 

 ADC_Init(ADC1,&ADC_InitStructure);

 

 

 

 ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;

 

 ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;

 

 ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;

 

 ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;

 

 ADC_CommonInit(&ADC_CommonInitStructure);

 

 

 

 ADC_RegularChannelConfig(ADC1,ADC_Channel_10,1,ADC_SampleTime_480Cycles);

 

 ADC_RegularChannelConfig(ADC1,ADC_Channel_11,2,ADC_SampleTime_480Cycles);

 

 ADC_RegularChannelConfig(ADC1, ADC_Channel_12, 3, ADC_SampleTime_480Cycles);

 

 

 

 

 

 /**

 

   Configure the DMA

 

 */

 

 //==Configure DMA2 - Stream 4

 

 DMA_DeInit(DMA2_Stream4);  //Set DMA registers to default values

 

 DMA_InitStructure.DMA_Channel = DMA_Channel_0;

 

 DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&ADC1->DR; //Source address

 

 DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&ADCConvertedValues[0]; //Destination address

 

 DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;

 

 DMA_InitStructure.DMA_BufferSize = MAX_ADC_CHANNELS; //Buffer size

 

 DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;

 

 DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;

 

 DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; //source size - 16bit

 

 DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord; // destination size = 16b

 

 DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;

 

 DMA_InitStructure.DMA_Priority = DMA_Priority_High;

 

 DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable;

 

 DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;

 

 DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;

 

 DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;

 

 DMA_Init(DMA2_Stream4, &DMA_InitStructure); //Initialize the DMA

 

 DMA_Cmd(DMA2_Stream4, ENABLE); //Enable the DMA2 - Stream 4

 

 while(DMA_GetCmdStatus(DMA2_Stream4)==DISABLE){};

 

 

 

 ADC_DMARequestAfterLastTransferCmd(ADC1, ENABLE);

 

 ADC_DMACmd(ADC1, ENABLE); //Enable ADC1 DMA

 

 ADC_Cmd(ADC1, ENABLE);   // Enable ADC1

 

 ADC_ContinuousModeCmd(ADC1,ENABLE);

 

 ADC_SoftwareStartConv(ADC1); // Start ADC1 conversion

 

}

 

 

 

 

 

int main(void)

 

{

 

adc_dma_init();

 

    while(1)

 

    {

 

 

 

            ADC1_Conversion(0);

 

            ADC1_Conversion(1);

 

            ADC1_Conversion(2);

 

     

 

    }

 

}

A

ny one can suggest what may cause the issue for this.

regards

kudiarasu

 

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on June 29, 2015 at 19:14

Any one can suggest what may cause the issue for this.

The asserted state is not RESET?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
kudiarasum
Associate II
Posted on June 30, 2015 at 08:40

Thanks Clive1,

Now i have changed like below

while (!DMA_GetFlagStatus(DMA2_Stream4,DMA_FLAG_TCIF4));

and control moves beyond this.

But i have another issue, As mentioned in my previous post,

 i have reading the ADC channels PC0, PC1 &PC2 which actually connected 2.7volts to all three pins in my stm32f407 discovery board and i am expecting 3350 as a result.

But result seems to be erratic and it reads 4095,4095,0 as a results . i thing  did some mistakes in adc dma initialization . possible can you review my adc dma initialization  code ?

Thanks in advance

kudiarasu.

Posted on June 30, 2015 at 17:07

Skimming through it looks reasonable enough, not how I'd do it, but I've posted working examples.

PC0 has some potential issues on the STM32F4-DISCO, PC1,PC2 seem free. TC fires when all three samples are ready.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..