Skip to main content
stankovic
Associate II
March 8, 2008
Question

UART with 8MHz internal oscillator?

  • March 8, 2008
  • 2 replies
  • 783 views
Posted on March 08, 2008 at 15:55

UART with 8MHz internal oscillator?

    This topic has been closed for replies.

    2 replies

    obtronix
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:26

    my opinion is I wouldn't make a commercial device using the STM32 internal osc to drive a UART without some type of calibration scheme, just my opinion!

    stankovic
    stankovicAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:26

    Hi,

    I am working on new board that has restriction in dimension (something new? :o) and think about using only internal oscillator(8MHz).

    OK, may be 32kHz for RTC if I can make it without external RTC chip (there is one ST software example about this, still need to read and test it).

    My question is - is it possible to make USART working (max. baud rate 57600) with internal oscillator?

    By STM32F103 datasheet max. oscillator error is +-3% (for -40,+105C), which is close to max. baud rate error allowed for UART.

    As I expect that device will be all the time in range -20, +80C oscillator error is probably lower.

    Also, anyone worked with CAN - what is tolerance there?

    This is not so critical as I am considering SPI as alternative, distance is quite short - max 20 cm.

    Thanks.