cancel
Showing results for 
Search instead for 
Did you mean: 

Tutorial 1 for STM32CUBEF4 did not work

s23
Associate
Posted on June 19, 2014 at 23:06

Hi,

I am following the instruction on UM1718 user manual, the section on Tutorial 1 from pinout to project C code generation using an STM32F4MCU). The following listed the codes generated by the code generator. I have added code as instructed by the user manual. However, nothing works. Can anyone help, please?

Thanks

/* Includes ------------------------------------------------------------------*/

#include ''stm32f4xx_hal.h''

/* Private variables ---------------------------------------------------------*/

TIM_HandleTypeDef htim3;

/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/* Private function prototypes -----------------------------------------------*/

static void SystemClock_Config(void);

static void MX_GPIO_Init(void);

static void MX_TIM3_Init(void);

int main(void)

{

  /* USER CODE BEGIN 1 */

  /* USER CODE END 1 */

  /* MCU Configuration----------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */

  HAL_Init();

  /* Configure the system clock */

  SystemClock_Config();

  /* Initialize all configured peripherals */

  MX_GPIO_Init();

  MX_TIM3_Init();

  /* USER CODE BEGIN 2 */

  /* USER CODE END 2 */

  /* USER CODE BEGIN 3 */

 

  HAL_TIM_Base_Start(&htim3);

  

  /* Infinite loop */

  while (1)

  {

  

  }

  /* USER CODE END 3 */

}

/** System Clock Configuration

*/

static void SystemClock_Config(void)

{

  RCC_OscInitTypeDef RCC_OscInitStruct;

  __PWR_CLK_ENABLE();

  __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);

  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;

  RCC_OscInitStruct.HSIState = RCC_HSI_ON;

  RCC_OscInitStruct.HSICalibrationValue = 6;

  HAL_RCC_OscConfig(&RCC_OscInitStruct);

}

/* TIM3 init function */

void MX_TIM3_Init(void)

{

  TIM_ClockConfigTypeDef sClockSourceConfig;

  TIM_MasterConfigTypeDef sMasterConfig;

  htim3.Instance = TIM3;

  htim3.Init.Prescaler = 16000;

  htim3.Init.CounterMode = TIM_COUNTERMODE_UP;

  htim3.Init.Period = 1000;

  htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

  HAL_TIM_Base_Init(&htim3);

  sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;

  HAL_TIM_ConfigClockSource(&htim3, &sClockSourceConfig);

  sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;

  sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;

  HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig);

}

/** Configure pins as 

        * Analog 

        * Input 

        * Output

        * EVENT_OUT

        * EXTI

*/

void MX_GPIO_Init(void)

{

  GPIO_InitTypeDef GPIO_InitStruct;

  /* GPIO Ports Clock Enable */

  __GPIOD_CLK_ENABLE();

  /*Configure GPIO pin : PD12 */

  GPIO_InitStruct.Pin = GPIO_PIN_12;

  GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;

  GPIO_InitStruct.Pull = GPIO_NOPULL;

  GPIO_InitStruct.Speed = GPIO_SPEED_LOW;

  HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

}

/* USER CODE BEGIN 4 */

void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)

{    

   if (htim->Instance==htim3.Instance) HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_12);

}

/* USER CODE END 4 */

#ifdef USE_FULL_ASSERT

/**

   * @brief Reports the name of the source file and the source line number

   * where the assert_param error has occurred.

   * @param file: pointer to the source file name

   * @param line: assert_param error line source number

   * @retval None

   */

void assert_failed(uint8_t* file, uint32_t line)

{

  /* User can add his own implementation to report the file name and line number,

    ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */

}

#endif

/**

  * @}

  */ 

/**

  * @}

*/ 

/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
stm32cube-t
ST Employee
Posted on June 24, 2014 at 21:23

Hello,

Replace in your code : HAL_TIM_Base_Start(&htim1); 

with: HAL_TIM_Base_Start_IT(&htim3);  (as stated in the user manual)

Ensure also the proper configuration of the interrupts: in MX configuration tab, check under NVIC settings, TIM3 global interrupt is enabled and set a priority (ex: 15).