cancel
Showing results for 
Search instead for 
Did you mean: 

Transfer of Right Aligned ADC data to the User defined variable using multiple channels ADC (STM32F4)

Engineering Student91
Associate II
Posted on November 28, 2017 at 16:53

Dear all,

I have configured ADC - 1 channel with DMA to retrieve data. It all works fine. 

Now, I am trying to use the same ADC (ADC1, DMA2_Stream0) to use 2 channels (channel 12 and 13). 

uint16_t ADC_Value[2] = {0,0}; //the user variable for retrieving ADC data from 2 channels

 DMA_InitStructure.DMA_Channel =DMA_Channel_0;

 DMA_InitStructure.DMA_PeripheralBaseAddr =(uint32_t)&ADC1->DR;

 DMA_InitStructure.DMA_Memory0BaseAddr =(uint32_t)&ADC_Value;

 DMA_InitStructure.DMA_DIR =DMA_DIR_PeripheralToMemory;

 DMA_InitStructure.DMA_BufferSize =2; // increase the buffer size for multi-channels

 DMA_InitStructure.DMA_PeripheralInc =DMA_PeripheralInc_Disable;

 DMA_InitStructure.DMA_MemoryInc =DMA_MemoryInc_Enable; //Enabling the memory increment

 DMA_InitStructure.DMA_PeripheralDataSize =DMA_PeripheralDataSize_HalfWord;

 DMA_InitStructure.DMA_MemoryDataSize =DMA_MemoryDataSize_HalfWord;

 DMA_InitStructure.DMA_Mode =DMA_Mode_Circular;

 DMA_InitStructure.DMA_Priority =DMA_Priority_High;

 DMA_InitStructure.DMA_FIFOMode =DMA_FIFOMode_Disable;

 DMA_InitStructure.DMA_FIFOThreshold =DMA_FIFOThreshold_HalfFull;

 DMA_InitStructure.DMA_MemoryBurst =DMA_MemoryBurst_Single;

 DMA_InitStructure.DMA_PeripheralBurst =DMA_PeripheralBurst_Single;

 DMA_Init(DMA2_Stream0, &DMA_InitStructure);

 DMA_Cmd(DMA2_Stream0, ENABLE);

 /* ADC1 Init ****************************************************************/

 ADC_InitStructure.ADC_Resolution =ADC_Resolution_12b;

 ADC_InitStructure.ADC_ScanConvMode =ENABLE;  // Single channel or Multiple channels (ENABLE)

 ADC_InitStructure.ADC_ContinuousConvMode =ENABLE;

 ADC_InitStructure.ADC_ExternalTrigConvEdge =ADC_ExternalTrigConvEdge_None; //Software Conversion

 ADC_InitStructure.ADC_ExternalTrigConv =ADC_ExternalTrigConv_T1_CC1;

 ADC_InitStructure.ADC_DataAlign =ADC_DataAlign_Right;

 ADC_InitStructure.ADC_NbrOfConversion =2; // INCREASE for multiple channels

 ADC_Init(ADC1, &ADC_InitStructure);

In the main(),

while(1)

{

printf('%d,%d,%d\r\n',ADC_Value[0],ADC_Value[1],myCounter);

}

Firstly, I'd like to know if my settings are correct. And secondly, Can someone explain me how exactly the result variable (array) is filled with ADC data from the DR? 

Thanks a lot.

#adc-dma-stm32f4 #adc
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on November 28, 2017 at 17:44

Doesn't the RM describe the process? One 16-bit word at a time, triggered by EOC of channel.

Variable should be volatile, DMA changes outside execution flow.

You'd need two ADC to sample at the same time, then you'd use CDR (Common Data Register), which basically combines ADC1->DR and ADC2->DR into a singular 32-bit read.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..