cancel
Showing results for 
Search instead for 
Did you mean: 

transfer 8btt data using GPIO 8 ports with CLK 42MHz

dukesong
Associate II
Posted on February 05, 2015 at 12:18

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on February 05, 2015 at 14:48

This is your THIRD thread on this topic.

Like I told you yesterday, you'd need to write WORDs to the GPIO->ODR, and you'd need those correctly BIT aligned with the pins you're using.

42 MHz seems very optimistic, people doing this professionally would choose an FPGA, or hardware to do this.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on February 05, 2015 at 14:55

And this is with just 4 posts

[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32F427%20data%20transfer%20from%20GPIO%208port%20using%20DMA%20to%20other%20board&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&currentviews=21]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fSTM32F427%20data%20transfer%20from%20GPIO%208port%20using%20DMA%20to%20other%20board&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=21

[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32F427%20data%20transfer%20from%20GPIO%208port%20using%20DMA%20to%20other%20board&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&currentviews=21]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fSTM32F427%20data%20transfer%20from%20GPIO%208port%20using%20DMA%20to%20other%20board&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=21

I've posted examples of DMA to/from GPIO pins, using internal/external clocks. Suggest some Google Foo, and serious consideration of what you're doing.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..