cancel
Showing results for 
Search instead for 
Did you mean: 

Tracking down a UsageFault origin on an STM32F303

kevinhuang
Associate II
Posted on February 11, 2015 at 02:44

Greetings,

I'm working with an STM32F303 MCU. On one of my projects, I've noticed that it would repeatedly freeze up, requiring a reset to continue operation. Doing a backtrace shows me that the error originates from this piece of code:

/* CRC16 implementation acording to CCITT standards */
static
const
uint16_t crc16tab[256] = {
0x0000, 0x1021, 0x2042, 0x3063, 0x4084, 0x50A5, 0x60C6, 0x70E7,
0x8108, 0x9129, 0xA14A, 0xB16B, 0xC18C, 0xD1AD, 0xE1CE, 0xF1EF,
0x1231, 0x0210, 0x3273, 0x2252, 0x52B5, 0x4294, 0x72F7, 0x62D6,
0x9339, 0x8318, 0xB37B, 0xA35A, 0xD3BD, 0xC39C, 0xF3FF, 0xE3DE,
0x2462, 0x3443, 0x0420, 0x1401, 0x64E6, 0x74C7, 0x44A4, 0x5485,
0xA56A, 0xB54B, 0x8528, 0x9509, 0xE5EE, 0xF5CF, 0xC5AC, 0xD58D,
0x3653, 0x2672, 0x1611, 0x0630, 0x76D7, 0x66F6, 0x5695, 0x46B4,
0xB75B, 0xA77A, 0x9719, 0x8738, 0xF7DF, 0xE7FE, 0xD79D, 0xC7BC,
0x48C4, 0x58E5, 0x6886, 0x78A7, 0x0840, 0x1861, 0x2802, 0x3823,
0xC9CC, 0xD9ED, 0xE98E, 0xF9AF, 0x8948, 0x9969, 0xA90A, 0xB92B,
0x5AF5, 0x4AD4, 0x7AB7, 0x6A96, 0x1A71, 0x0A50, 0x3A33, 0x2A12,
0xDBFD, 0xCBDC, 0xFBBF, 0xEB9E, 0x9B79, 0x8B58, 0xBB3B, 0xAB1A,
0x6CA6, 0x7C87, 0x4CE4, 0x5CC5, 0x2C22, 0x3C03, 0x0C60, 0x1C41,
0xEDAE, 0xFD8F, 0xCDEC, 0xDDCD, 0xAD2A, 0xBD0B, 0x8D68, 0x9D49,
0x7E97, 0x6EB6, 0x5ED5, 0x4EF4, 0x3E13, 0x2E32, 0x1E51, 0x0E70,
0xFF9F, 0xEFBE, 0xDFDD, 0xCFFC, 0xBF1B, 0xAF3A, 0x9F59, 0x8F78,
0x9188, 0x81A9, 0xB1CA, 0xA1EB, 0xD10C, 0xC12D, 0xF14E, 0xE16F,
0x1080, 0x00A1, 0x30C2, 0x20E3, 0x5004, 0x4025, 0x7046, 0x6067,
0x83B9, 0x9398, 0xA3FB, 0xB3DA, 0xC33D, 0xD31C, 0xE37F, 0xF35E,
0x02B1, 0x1290, 0x22F3, 0x32D2, 0x4235, 0x5214, 0x6277, 0x7256,
0xB5EA, 0xA5CB, 0x95A8, 0x8589, 0xF56E, 0xE54F, 0xD52C, 0xC50D,
0x34E2, 0x24C3, 0x14A0, 0x0481, 0x7466, 0x6447, 0x5424, 0x4405,
0xA7DB, 0xB7FA, 0x8799, 0x97B8, 0xE75F, 0xF77E, 0xC71D, 0xD73C,
0x26D3, 0x36F2, 0x0691, 0x16B0, 0x6657, 0x7676, 0x4615, 0x5634,
0xD94C, 0xC96D, 0xF90E, 0xE92F, 0x99C8, 0x89E9, 0xB98A, 0xA9AB,
0x5844, 0x4865, 0x7806, 0x6827, 0x18C0, 0x08E1, 0x3882, 0x28A3,
0xCB7D, 0xDB5C, 0xEB3F, 0xFB1E, 0x8BF9, 0x9BD8, 0xABBB, 0xBB9A,
0x4A75, 0x5A54, 0x6A37, 0x7A16, 0x0AF1, 0x1AD0, 0x2AB3, 0x3A92,
0xFD2E, 0xED0F, 0xDD6C, 0xCD4D, 0xBDAA, 0xAD8B, 0x9DE8, 0x8DC9,
0x7C26, 0x6C07, 0x5C64, 0x4C45, 0x3CA2, 0x2C83, 0x1CE0, 0x0CC1,
0xEF1F, 0xFF3E, 0xCF5D, 0xDF7C, 0xAF9B, 0xBFBA, 0x8FD9, 0x9FF8,
0x6E17, 0x7E36, 0x4E55, 0x5E74, 0x2E93, 0x3EB2, 0x0ED1, 0x1EF0
};
/** Calculate CCITT 16-bit Cyclical Redundancy Check (CRC16).
*
* This implementation uses parameters used by XMODEM i.e. polynomial is:
* \f[
* x^{16} + x^{12} + x^5 + 1
* \f]
* Mask 0x11021, not reversed, not XOR'd
* (there are several slight variants on the CCITT CRC-16).
*
* \param buf Array of data to calculate CRC for
* \param len Length of data array
* \param crc Initial CRC value
*
* \return CRC16 value
*/
uint16_t crc16_ccitt(uint8_t *buf, uint16_t len, uint16_t crc)
{
uint16_t i;
for
(i = 0; i < len; i++)
{
crc = (crc << 8) ^ crc16tab[((crc >> 8) ^ *buf++) & 0x00FF];
}
return
crc;
}

I use this checksum repeatedly without any major issue, so I'm skeptical that it's the software. Using GDB I printed out the contents of the CFSR register, which returned 0x8200, which indicates that a precise bus error had occurred, and the contents of BFAR points to a valid address. Printing out the contents of BFAR gives me 0x2000A000. By my understanding, 0x20000000 is where SRAM begins, so I assume this is just data? At this point I'm at a loss for figuring out what caused the error. This bug has been difficult to characterize because the error occurs seemingly randomly between minutes of a reset or up to several hours. Has anyone else had any experience with debugging something like this, and do you have any suggestions of other things to check? Thanks #stm32f3
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on February 11, 2015 at 05:15

So how large is the RAM in your specific part? How big is the stack/heap?

The problem is likely with the buffers being passed into the routine. Look at how those are allocated, where they come from. Put some sanity checking on the buffer/size parameters as it enters, checking if they exceed the memory footprint of your device. Then work back to understand where the bogus buffers are coming from.

Understand clearly your current stack utilization. Fill it with a known character/pattern and periodically review how deep it's gotten.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
kevinhuang
Associate II
Posted on February 12, 2015 at 00:55

The specific chip I'm using is the STM32F303VCT6, which should give me 40K of RAM.  I've now made the connection that the start address of the stack is 0x2000A000. I've added a print statement to print out the address of ''i'' that was in the previous code above, which I believe should be a reasonable indicator for where the stack is at. So far it's reporting that the local variable is located at 0x20009fbe, and this remains very consistent. So it seems like my stack doesn't really grow past this point (70-ish bytes). 

The function gets called from two separate places. The first place passed in a buffer that was declared in the global space. The other one was an array declared locally, so that falls on the stack. I've moved it to the global namespace as well and now i'm retesting the code to see if this error reoccurs. I'm also printing out the passed-in length of the buffer and the stack size when the function gets called. Hopefully moving the previously mentioned array to the global space fixed things, but if it crashes again, hopefully I'll get a better idea of what caused the crash. 

waclawek.jan
Super User
Posted on February 12, 2015 at 10:05

IMO you are calling the CRC routine with invalid unbounded length, e.g. coming from erratic communication.

JW