cancel
Showing results for 
Search instead for 
Did you mean: 

Timers with F4 DISCO

botmail2422
Associate II
Posted on June 23, 2016 at 21:54

I want to measure how long a signal is high as accurately as possible (preferably down to the microsecond). I started by triggering an EXTI interrupt one both the rising and falling edge of the signal. The EXTI handler would check if the signal is high or low. If high, it would start a timer, and if low it would end it and return how long the timer was active. I tried to implement this with SysTick but I fear it is not accurate enough. I thought about using a TIM but I don't know how to return how long the timer was running... Any advice?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on June 23, 2016 at 22:16

For a continuous signal, I'd use PWM Input mode, otherwise Input Capture where Channel 1 and 2 were configured to timestamp opposite edges of the same signal.

On an F4, I'd use a 32-bit timer clocking between 84 MHz and 1 MHz, and compute the delta ticks between rising and falling edges..

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..