cancel
Showing results for 
Search instead for 
Did you mean: 

TIMER1_DMA Capture

surender2525
Associate II
Posted on March 07, 2016 at 12:25

Hi,

   I'm using STM32F103RC controller, trying to Capture Frequency from 1.2Khz to 72Mhz by using Timer-1 with DMA Channel-2.

i'm not able to capture a constant count from TIM1->CCR1, the count value keeps on varying.

In need of HELP.!

#include ''stm32f10x.h''

#define CFGR_REG_VAL     0x001D8402; 

#define System_CoreClock    72000000.0

void RCC_Configuration(void);

void Timer1_Master(void);

void GPIO_initailization(void);

void DMA1_Channel2_configuration(void);

unsigned short Memory[50];

main()

{

RCC_Configuration();

Timer1_Master();

GPIO_initailization();

DMA1_Channel2_configuration();

while(1);

}

/////////////////////////////CLOCK///////////////////////////////////////////

void RCC_Configuration(void)

{

RCC->CSR  |=  0x01000000;

RCC->CR    =  0x00010080; //external highe speed clock enabled

if ((RCC->CR & RCC_CR_HSEON)) 

{                 // if HSE enabled

while ((RCC->CR & RCC_CR_HSERDY)==0 ); // Wait for HSERDY = 1 (HSE is ready)

  //Flash access control reg

FLASH->ACR =  0x12 ; //prefetch buffer enabled and flash latency(2 wait state)

RCC->CFGR  =  CFGR_REG_VAL ;

RCC->CR   |=  0x01000000;   //PLL enable

  if (RCC->CR & RCC_CR_PLLON) 

  {                 // if PLL enabled

    while ((RCC->CR & RCC_CR_PLLRDY) == 0); // Wait for PLLRDY = 1 (PLL is ready)

  }

while ((RCC->CFGR & 0x0000008) ==0);

}      

void GPIO_initailization(void)

{   

RCC->APB2ENR |= 0x00000001;        /**** enable afio ******/

RCC->APB2ENR |= 0x0000000C;       /**** enable gpio A & B ******/

GPIOA->CRH     = 0x00000004;       /* TIMER 1 PIN 41 FOR capture INPUT  floating*/

}

//////////////////////////////TIMER1/////////////////////////////////

void Timer1_Master(void)   

RCC->APB2ENR |= 0x0800; // clock of TIM1

TIM1->PSC = 0x0000; // PSC = 1 (i.e 72MHZ/1)

TIM1->ARR = 0xffff; // Autoreload value (65535)

TIM1->CNT = 0x0000; // Counter value  

TIM1->EGR = 0X0002; // Counter is captured in TIMx_CCR1 register

TIM1->CCMR1 = 0x0031; // 01: CC1 channel is configured as input, IC1 is mapped on TI1 0011: fSAMPLING=fCK_INT, N=8

TIM1->CR2 = 0x0008; // 1: CCx DMA requests sent when update event occurs

TIM1->DIER = 0x0200; // Capture/Compare 1 interrupt enable, Capture/Compare 1 DMA request enable

TIM1->CR1 = 0x0001; // 1: Only counter overflow/underflow generates an update interrupt or DMA request if enabled.URS bit is eanbled

TIM1->CCER = 0x0001; // Capture/Compare 1 input enable

void DMA1_Channel2_configuration(void)

{

    RCC->AHBENR = (RCC->AHBENR & 0xFFFFFFF6) | 0x00000001;// DMA1 clk enable

DMA1_Channel2->CPAR = (int)&TIM1->CCR1; // PERIPHERAL address

DMA1_Channel2->CMAR = (int)&Memory;                          // memory address

DMA1_Channel2->CNDTR = 50;   // number of data

DMA1_Channel2->CCR = (0xFFEF & DMA1_Channel2->CCR) | 0x00 ; //  read from peripheral 

DMA1_Channel2->CCR = (0xFFDF & DMA1_Channel2->CCR) | 0x20 ;        //   circular mode enable

DMA1_Channel2->CCR = (0xFF7F & DMA1_Channel2->CCR) | 0x80 ;       //   memory inc mode

DMA1_Channel2->CCR |= 0x200; // high priority level

DMA1_Channel2->CCR |= 0x500;   //peripheral size 16-bits and memory size 16-bits

DMA1_Channel2->CCR |= 0x01;                                        // channel enable

}

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
Posted on March 07, 2016 at 19:03

Well Input Capture just copies the value in TIMx->CNT into TIMx->CCRx, the counting element ticks at the rate of the timer described by the time base.

Typically you'd take TWO measurements and subtract them from each other to get a delta count in the ticks of the time base clock.

ie a 50 Hz signal might report 10000, then 30000, then 50000, ie a delta of 20000 ticks of a clock of 1 MHz (1 us)

20000us = 20ms = 0.02s,

1/50 = 0.02 s

If you want the counter to reset you'd need to use PWM Input mode.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
surender2525
Associate II
Posted on March 08, 2016 at 10:53

The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6pU&d=%2Fa%2F0X0000000bwN%2Fu7l5HQ7Q_nNQD.Hr4Xn85KW5qOCyXJ7_qXEiCtkXfCk&asPdf=false
surender2525
Associate II
Posted on March 08, 2016 at 15:21

But, i'm not able to capture the same Count in DMA.!

Well the DMA can read TIM1->CCR1, it can't write TIM1->CNT = 0, so it's not going to do the same thing, is it? Also don't use the ' TIM1->SR &= ' form, just write the mask to clear the interrupt.

Review the use of PWM Input mode

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
surender2525
Associate II
Posted on March 09, 2016 at 11:26

PWM INPUT MODE

Thanks a lot ''Clive1''. It was verymuch Helpful.

Now, It capture's the Constant count by using

PWM INPUT MODE

in Timer1 DMA..

Another Doubt,

Can we Cascade 2 Timers ( i.e Timer-1 Master cascade with Timer-2 Slave) and 

Capture Frequency from 0 to 50Mhz using DMA?

I've used Timer IRQ. To get the Capture Count in IRQ,were MSB value in 

Timer 1 TIM1->CCR1; and LSB value in Timer 2 TIM2->CNT; )

That is,

Frequency Count =  TIM1->CCR1 +  (TIM2->CNT*65535);

But in DMA1_Channel2->CPAR,  if we use 2 Timers, which PERIPHERAL dress should be given?

surender2525
Associate II
Posted on March 09, 2016 at 11:30

PWM INPUT MODE

Thanks a lot ''Clive1''. It was verymuch Helpful.

Now, It capture's the Constant count by using

PWM INPUT MODE

in Timer1 DMA..

Another Doubt,

Can we Cascade 2 Timers ( i.e Timer-1 Master cascade with Timer-2 Slave) and 

Capture Frequency from 0 to 50Mhz using DMA?

I've used Timer IRQ. To get the Capture Count in IRQ,were MSB value in

Timer 1 TIM1->CCR1; and LSB value in Timer 2 TIM2->CNT; )

That is,

Frequency Count =  TIM1->CCR1 +  (TIM2->CNT*65535);

But in DMA1_Channel2->CPAR,  if we use 2 Timers, which PERIPHERAL dress should be given?