cancel
Showing results for 
Search instead for 
Did you mean: 

TIM1 Input Capture

johnbeck9
Associate II
Posted on May 19, 2009 at 11:37

TIM1 Input Capture

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
johnbeck9
Associate II
Posted on May 17, 2011 at 13:11

Does anyone have a good example of simple input capture using timer 1?

(I have been struggling for quite awhile on something that should be really simple.)

Here is my senario

PE9 TIM1_CH1 has between 10-100Hz signal

PE11 TIM1_CH2 has between 15-100Hz signal

PE13 TIM1_CH3 has between 15-100Hz signal

PE11 TIM1_CH4 has between 50-200Hz signal

RCC_APB2 = 72Mhz

Code snippets (can't seem to get an interrupt on TIM1_CC_IRQHandler)

What am I missing?

// 16Mhz crystal

void RCC_Configuration(void)

{

/* RCC system reset(for debug purpose) */

RCC_DeInit();

/* Enable HSE */

RCC_HSEConfig(RCC_HSE_ON); //jjb

// RCC_HSEConfig(RCC_HSE_OFF);

/* Wait till HSE is ready */

HSEStartUpStatus = RCC_WaitForHSEStartUp();

if(HSEStartUpStatus == SUCCESS)

{

/* Enable Prefetch Buffer */

FLASH_PrefetchBufferCmd(FLASH_PrefetchBuffer_Enable);

/* Flash 2 wait state */

FLASH_SetLatency(FLASH_Latency_2);

/* HCLK = SYSCLK */

RCC_HCLKConfig(RCC_SYSCLK_Div1);

/* PCLK2 = HCLK */

RCC_PCLK2Config(RCC_HCLK_Div1);

/* PCLK1 = HCLK/2 */

RCC_PCLK1Config(RCC_HCLK_Div2);

/* PLLCLK = 8MHz * 9 = 72 MHz */

RCC_PLLConfig(RCC_PLLSource_HSE_Div2, RCC_PLLMul_9);

/* Enable PLL */

RCC_PLLCmd(ENABLE);

/* Wait till PLL is ready */

while(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET)

{

}

/* Select PLL as system clock source */

RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK);

/* Wait till PLL is used as system clock source */

while(RCC_GetSYSCLKSource() != 0x08)

{

}

}

RCC_APB1PeriphClockCmd( RCC_APB1Periph_TIM2 |

RCC_APB1Periph_TIM3 |

RCC_APB1Periph_TIM4 |

RCC_APB1Periph_I2C1 |

RCC_APB1Periph_USART2 |

RCC_APB1Periph_USART3 ,

ENABLE

);

RCC_APB2PeriphClockCmd( RCC_APB2Periph_GPIOA |

RCC_APB2Periph_GPIOB |

RCC_APB2Periph_GPIOC |

RCC_APB2Periph_GPIOD |

RCC_APB2Periph_GPIOE |

RCC_APB2Periph_GPIOF |

RCC_APB2Periph_GPIOG |

RCC_APB2Periph_TIM1 |

RCC_APB2Periph_USART1 |

RCC_APB2Periph_AFIO ,

ENABLE

);

}

____________________________________________________________

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_2MHz;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;

GPIO_InitStructure.GPIO_Pin = FAN1_4_TACH | FAN5_8_TACH | FAN9_12_TACH | PUMP_TACH; // PE9,11,13,14

GPIO_Init(TACH_READ_PORT, &GPIO_InitStructure); // pE9

GPIO_PinRemapConfig(GPIO_FullRemap_TIM1, ENABLE);

__________________________________________________________

TIM_ICInitTypeDef TIM_ICInitStructure;

TIM_ICInitStructure.TIM_Channel = TIM_Channel_1; TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising; TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI; TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1; TIM_ICInitStructure.TIM_ICFilter = 0x0; TIM_ICInit(TIM1, &TIM_ICInitStructure);

/* Enable the CCxInterrupt Request */

TIM_ITConfig(TIM1, TIM_IT_CC1, ENABLE);

TIM_ITConfig(TIM1, TIM_IT_CC2, ENABLE);

TIM_ITConfig(TIM1, TIM_IT_CC3, ENABLE);

TIM_ITConfig(TIM1, TIM_IT_CC4, ENABLE);

__________________________________

/* Enable the TIM1 Interrupt */

NVIC_InitStructure.NVIC_IRQChannel = TIM1_CC_IRQChannel;

NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1;

NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;

NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&NVIC_InitStructure);

________________________________________

void TIM1_CC_IRQHandler(void)

{

vu16 IC2Value = 0;

vu16 DutyCycle = 0;

vu32 Frequency = 0;

static ccIT;

if (TIM_GetITStatus(TIM1, TIM_IT_CC1)){

ccIT = 1;

}

if (TIM_GetITStatus(TIM1, TIM_IT_CC2)){

ccIT = 2;

}

if (TIM_GetITStatus(TIM1, TIM_IT_CC3)){

ccIT = 4;

}

if (TIM_GetITStatus(TIM1, TIM_IT_CC4)){

ccIT = 8;

}

/* Clear TIM1 Capture compare interrupt pending bit */

TIM_ClearITPendingBit(TIM1, TIM_IT_CC4);

/* Get the Input Capture value */

IC2Value = TIM_GetCapture4(TIM1);

if (IC2Value != 0)

{

/* Duty cycle computation */

DutyCycle = (TIM_GetCapture1(TIM1) * 100) / IC2Value;

/* Frequency computation */

Frequency = 72000000 / IC2Value;

}

else

{

DutyCycle = 0;

Frequency = 0;

}

}

amin2
Associate II
Posted on May 17, 2011 at 13:11

Hi ,

since the STM8S and STM32 Timers are very similar, I advice you to take a look on the STM8S Firmware Timer example named ''TIM1_Input_Capture''.

Amin

---------------------

/* Private typedef -----------------------------------------------------------*/

/* Private define ------------------------------------------------------------*/

/* Private macro -------------------------------------------------------------*/

/* Private variables ---------------------------------------------------------*/

u32 TIM1ClockFreq = 2000000;

u32 LSIClockFreq = 0;

u16 ICValue1 =0, ICValue2 =0;

/* Private function prototypes -----------------------------------------------*/

/* Private functions ---------------------------------------------------------*/

/* Public functions ----------------------------------------------------------*/

/**

* @brief Example firmware main entry point.

* @par Parameters:

* None

* @retval void None

* @par Required preconditions:

* None

*/

void main(void)

{

TIM1_ICInit( TIM1_CHANNEL_1, TIM1_ICPOLARITY_FALLING, TIM1_ICSELECTION_DIRECTTI, TIM1_ICPSC_DIV8, 0x0);

/* Enable CC1 interrupt */

TIM1_ITConfig(TIM1_IT_CC1, ENABLE);

/* Enable TIM1 */

TIM1_Cmd(ENABLE);

/* Clear CC1 Flag*/

TIM1_ClearFlag(TIM1_FLAG_CC1);

/* Connect LSI to COO pin*/

GPIO_Init(GPIOE, GPIO_PIN_0, GPIO_MODE_OUT_PP_LOW_FAST);

CLK_CCOConfig(CLK_OUTPUT_LSI);

CLK_CCOCmd(ENABLE);

/* wait a capture on CC1 */

while((TIM1->SR1 & TIM1_FLAG_CC1) != TIM1_FLAG_CC1);

/* Get CCR1 value*/

ICValue1 = TIM1_GetCapture1();

TIM1_ClearFlag(TIM1_FLAG_CC1);

/* wait a capture on cc1 */

while((TIM1->SR1 & TIM1_FLAG_CC1) != TIM1_FLAG_CC1);

/* Get CCR1 value*/

ICValue2 = TIM1_GetCapture1();

TIM1_ClearFlag(TIM1_FLAG_CC1);

/* Compute LSI clock frequency */

LSIClockFreq = (8 * TIM1ClockFreq) / (ICValue2 - ICValue1);

/* Insert a break point here */

while (1);

}

johnbeck9
Associate II
Posted on May 17, 2011 at 13:11

Thanks