2012-06-14 1:00 AM
Hi all,
I'm working on a project with a dumb TFT LCD (320 x 240). I'm trying to display static images (no double buffer). I've been able to display images (in 565 format) that I load on the flash memory and refresh it on the display using DMA and FSMC. I'm now trying to refresh the same images from external RAM using DMA again but I don't seem to get it right. What I'm doing is copying the images from the flash to the external RAM using DMA and then refresh from the external RAM.I thought maybe I wasn't writing to external RAM, I tried to view what's inside the external RAM after writing and I was able to see the same data that is on flash.I based my approach on the AN3241.Can you guys please help me to see what I'm doing wrong.Thank you #fsmc-dma-external-sram-psram #fsmc-dma-external-ram-tft-lcd2013-09-10 11:33 AM
The 429 is a different beast, with a LCD and SDRAM controller, I'd want to see a couple of board implementation as the potential for pin clashes is still very high.
Although I'm still a little confused about the clocking, as supposedly the CPU can go at 180 MHz, but the SDRAM is 84 MHz (168/2). Not sure how to get to 48 MHz from 180.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.