2010-12-03 4:09 AM
How to use built-in temperature detector? has anyone used it? any example?
I just found in the documentation that temperature detector is in ADC1_IN16 input channel. But how do I access it? I am green to the subject; just configured my row of LEDs to light on; I want to read temperature and output it on a row of LEDS.2010-12-04 10:22 AM
http://www.micromouseonline.com/blog/2009/05/25/simple-adc-use-on-the-stm32
http://www.micromouseonline.com/blog/2009/05/25/simple-adc-use-on-the-stm32
have a look, but modify the code taking care that max freq. for value line is 24 MHz instead of 72 MHz and ADC clock must be configured 12 MHz.brazov2
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.