Skip to main content
vinicius_acvasconcelos
Associate III
May 28, 2009
Question

Tachometer

  • May 28, 2009
  • 6 replies
  • 1824 views
Posted on May 28, 2009 at 16:54

Tachometer

    This topic has been closed for replies.

    6 replies

    jaroslaw2
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:12

    Try this:

    Code:

    <BR>TIM2->PSC=(u16)iPrescalerForPWMI; <BR>

    [ This message was edited by: jaroslaw.oska on 25-05-2009 14:38 ]

    vinicius_acvasconcelos
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:12

    I`m using the st code example ''PWM_Input''. It's working perfect, but the problem is the minimum frequency to measure is 1100Hz.

    I wanna to measure frequency starts with 10Hz. How can I modified this example to measure 10Hz, thre is any prescaler to devide the 72Mhz?

    The code:

    TIM_ICInitStructure.TIM_Channel = TIM_Channel_2;

    TIM_ICInitStructure.TIM_ICPolarity = TIM_ICPolarity_Rising;

    TIM_ICInitStructure.TIM_ICSelection = TIM_ICSelection_DirectTI;

    TIM_ICInitStructure.TIM_ICPrescaler = TIM_ICPSC_DIV1;

    TIM_ICInitStructure.TIM_ICFilter = 0x0;

    TIM_PWMIConfig(TIM2, &TIM_ICInitStructure);

    /* Select the TIM2 Input Trigger: TI2FP2 */

    TIM_SelectInputTrigger(TIM2, TIM_TS_TI2FP2);

    /* Select the slave Mode: Reset Mode */

    TIM_SelectSlaveMode(TIM2, TIM_SlaveMode_Reset);

    /* Enable the Master/Slave Mode */

    TIM_SelectMasterSlaveMode(TIM2, TIM_MasterSlaveMode_Enable);

    /* TIM enable counter */

    TIM_Cmd(TIM2, ENABLE);

    /* Enable the CC2 Interrupt Request */

    TIM_ITConfig(TIM2, TIM_IT_CC2, ENABLE);

    void TIM2_IRQHandler(void)

    {

    /* Clear TIM2 Capture compare interrupt pending bit */

    TIM_ClearITPendingBit(TIM2, TIM_IT_CC2);

    /* Get the Input Capture value */

    IC2Value = TIM_GetCapture2(TIM2);

    if (IC2Value != 0)

    {

    /* Frequency computation */

    velmotor = (72000000/ IC2Value);

    }

    else

    {

    velmotor= 0;

    }

    }

    Thanks.

    jaroslaw2
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:12

    Did you see function you've used?

    void TIM_PrescalerConfig(TIM_TypeDef* TIMx, u16 Prescaler, u16 TIM_PSCReloadMode)

    {

    /* Check the parameters */

    assert_param(IS_TIM_ALL_PERIPH(TIMx));

    assert_param(IS_TIM_PRESCALER_RELOAD(TIM_PSCReloadMode));

    /* Set the Prescaler value */

    TIMx->PSC = Prescaler;

    /* Set or reset the UG Bit */

    TIMx->EGR = TIM_PSCReloadMode;

    }

    vinicius_acvasconcelos
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:12

    I solved the problem :-] using a function to devide the tim clock, for 655535. Now the frequency step is around 0.016Hz. I'm able to measure the 40 Hz.

    TIM_PrescalerConfig(TIM2, 0x1987, TIM_PSCReloadMode_Immediate);

    TIM2_IRQHandler:

    /* Clear TIM2 Capture compare interrupt pending bit */

    TIM_ClearITPendingBit(TIM2, TIM_IT_CC2);

    /* Get the Input Capture value */

    IC2Value = TIM_GetCapture2(TIM2);

    velmotor = (11017.5975/ IC2Value);

    vinicius_acvasconcelos
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:12

    The PSC is used select the numbers of envents to capture, I wanna only one envent(the period to measure the frequency).

    Quote:

    On 25-05-2009 at 14:36, Anonymous wrote:

    Try this:

    Code:

    <BR><BR>TIM2->PSC=(u16)iPrescalerForPWMI; <BR><BR>

    [ This message was edited by: jaroslaw.oska on 25-05-2009 14:38 ]

    [ This message was edited by: vinicius_acvasconcelos on 25-05-2009 16:54 ]

    vinicius_acvasconcelos
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:12

    Quote:

    On 26-05-2009 at 07:06, Anonymous wrote:

    Did you see function you've used?

    void TIM_PrescalerConfig(TIM_TypeDef* TIMx, u16 Prescaler, u16 TIM_PSCReloadMode)

    {

    /* Check the parameters */

    assert_param(IS_TIM_ALL_PERIPH(TIMx));

    assert_param(IS_TIM_PRESCALER_RELOAD(TIM_PSCReloadMode));

    /* Set the Prescaler value */

    TIMx->PSC = Prescaler;

    /* Set or reset the UG Bit */

    TIMx->EGR = TIM_PSCReloadMode;

    }

    You are write. I had mistake PSC for IC1PS. The correct is change the PSC and not the IC prescaler.

    Thanks