2016-12-26 9:26 AM
Hello,
Here is my code for set and reset PA.3 for stm32f10x
#include <stdio.h>
#include <string.h>#include 'stm32f10x_gpio.h'#include 'stm32f10x_rcc.h'#include 'stm32f10x_tim.h'void delay(void){
int i,j; for(i=0;i<10000;i++) for(j=0;j<250;j++);}
int main(void){
GPIO_InitTypeDef GPStructure; RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA,ENABLE); GPStructure.GPIO_Mode=GPIO_Mode_Out_PP; GPStructure.GPIO_Pin=GPIO_Pin_3; GPStructure.GPIO_Speed=GPIO_Speed_50MHz; GPIO_Init(GPIOA,&GPStructure);while(1){GPIO_SetBits(GPIOA,GPIO_Pin_3);delay();delay();delay();delay();delay();delay();GPIO_ResetBits(GPIOA,GPIO_Pin_3);delay();delay();}}
Well, I expect to get output voltage greater than 2.82 for high output voltage level and 0 for low voltage level but I get 1.3 for high output voltage level in set states! However it works fine for other ports (PB , ...)
In addition, I test it for PA.15 but I get only 3.2 volt for set and reset!!!
what is my mistake?
Solved! Go to Solution.
2016-12-26 11:09 AM
Any details about the board you are testing this on?
The most likely reason would be that the pin is connected to something else which is driving the pin low, and in the PA15 case could it be used by the debugger interface?
2016-12-26 11:09 AM
Any details about the board you are testing this on?
The most likely reason would be that the pin is connected to something else which is driving the pin low, and in the PA15 case could it be used by the debugger interface?
2016-12-26 1:14 PM
Thanks dear Clive on , your are right.Another electrical component was driving the pin low.However the PA.15 is free and I don't use it. Should I deactivate a certain register?
2016-12-26 5:40 PM
For the debug pins, you'd need remap the SWD/JTAG functionality off them. The Standard Peripheral Library v3.5.0 has a JTAG/GPIO example