STMF4 Timer external clock mode 1
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-12-15 1:54 AM
Hi everyone,
i want to count the positive edges of a pulsesignal on PA6 using a Timer with external clock.
To test the functionality i generate the signal and outputport is PA8. PA8 is linked with PA6.
After several tries it still doesn't count and i don't know why anymore.
Thanks if anyone knows a hint
Here the most important parts of the code:
GPIO_InitStruct.Pin = GPIO_PIN_6;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; GPIO_InitStruct.Alternate = GPIO_AF2_TIM3; //Signal assigned to AF2 TIM3GPIO_InitStruct.Pin = GPIO_PIN_8;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_PULLDOWN; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);__TIM3_CLK_ENABLE();
hTim3.Instance = TIM3; hTim3.Init.Prescaler = 40; hTim3.Init.CounterMode = TIM_COUNTERMODE_UP; hTim3.Init.Period = 700; hTim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; hTim3.Init.RepetitionCounter = 0; HAL_TIM_Base_Init(&hTim3); TIM_ClockConfigTypeDef TimClock; TimClock.ClockSource = TIM_CLOCKSOURCE_TI1; //ETRMODE1 oder TI1 TimClock.ClockPolarity = TIM_CLOCKPOLARITY_RISING; //polarity of TIx clock source TimClock.ClockPrescaler = TIM_CLOCKPRESCALER_DIV1; HAL_TIM_ConfigClockSource(&hTim3,&TimClock);TIM_SlaveConfigTypeDef SlaveConfig;
SlaveConfig.SlaveMode = TIM_SLAVEMODE_EXTERNAL1; //External Source als Clock SlaveConfig.InputTrigger = TIM_TS_TI1FP1; // SlaveConfig.TriggerFilter = 0; //No filter needed SlaveConfig.TriggerPolarity = TIM_TRIGGERPOLARITY_RISING; //Counting on rising edge SlaveConfig.TriggerPrescaler = TIM_TRIGGERPRESCALER_DIV1; //No Prescaler HAL_TIM_SlaveConfigSynchronization(&hTim3, &SlaveConfig); HAL_TIM_Base_Start(&hTim3);while (1)
{ HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_RESET); HAL_Delay(50); HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_SET); HAL_Delay(50); iz++; ic = __HAL_TIM_GET_COUNTER(&hTim3); if (ic==50){ HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_SET); }}- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-12-15 3:15 AM
Have little experience in using a timer with external clock this way as I like to use peripheral for various usages at same time. Until someone gives the right way to do it, 2 alternative ways:
If the frequency of the rising edge is reasonable, use a TIMER with internal clock reference, then inject 1 to 4 signals to the CC channels of the timer. The timer will 'input capture' when a rise or fall edge occured, and using the corresponding interrupt, you can increase a counter (a global variable). This way, you can also check the duty cycle, compare between up to 4 signals, generate delayed pulses using the 'output compare' mode. (this can be fun to use an op-amp with dynamic switches to run an integrator for example).
Another alternative way is to use EXTI (this is the simplest way).
Good luck!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-12-15 4:49 AM
GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
I don't Cube: is this OK for AF?
JW