cancel
Showing results for 
Search instead for 
Did you mean: 

STME2F4 + WİFİ -SPWF01SA vs esp8266

ASSAAD.ASSAAD
Associate II
Posted on August 27, 2016 at 09:00

Hello All ; 

I am sorry if it is not the right forum to post ; 

In my project I need a wifi connection ;

My question : is how to choose the best wifi module of my application : 

we see that ST has a good wifi module 

http://www.st.com/content/st_com/en/products/wireless-connectivity/wi-fi/spwf01sa.html

 ; and we have other option esp8266 

but what is the advantage of each ? 

Anyone uses both could tell me the advantages of each please ? 

Thank you inadvantage 
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
ASSAAD.ASSAAD
Associate II
Posted on August 30, 2016 at 14:32

Any support here , please ? 

stm32forum
Associate II
Posted on August 30, 2016 at 14:41

Depends on your application.

With the SPWF01SA you need also an extra cpu.

I prefer the Esp8266, with Arduino ide you have it up and running in 10 minutes.

And also important there's a big community out there who can help you.

Posted on December 28, 2016 at 03:41

looking at the STM32F103REY6 chip on the SPWF01SA, it has 3 SPI's.  Are all 3 of these available to be programmed (I don't see them mentioned in the datasheet) or is it possible to use one of the SPI's MOSI/MISO,SCLK pins and then just use 3 separate GPIO's for the chip select CS pin for my 3 slaves?  I need to be able to run 3 SPI slaves, a 20x4 LCD screen and 3 triac relays thru optoisolators.  Is my SPI config possible on this chip/wifi module to get what I need out of it plus the wifi features or do I need to run another MCU along side this chip to do all this?