2018-09-04 1:22 AM
Hello,
I enter the shutdown mode with the following code statement
HAL_PWR_EnableWakeUpPin( PWR_WAKEUP_PIN1_LOW );
HAL_PWR_DisableWakeUpPin( PWR_WAKEUP_PIN2 );
HAL_PWR_DisableWakeUpPin( PWR_WAKEUP_PIN3 );
HAL_PWR_DisableWakeUpPin( PWR_WAKEUP_PIN4 );
HAL_PWR_DisableWakeUpPin( PWR_WAKEUP_PIN5 );
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUF1);
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUF2);
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUF3);
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUF4);
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUF5);
HAL_PWREx_DisableInternalWakeUpLine();
HAL_PWREx_EnterSHUTDOWNMode( );If I wake up the system with PWR_WAKEUP_PIN1, I set the GPIO15 from PORTH to high.
I initialized the PORT and GPIO (CubeMX generates the code).
The result is that the system is hanging. If I reset the GPIO to low before entering the shutdown mode, everything is working fine.
Am I missing something? Maybe someone can explain me if I doing something wrong.
Is there any bug know that happens when using shutdownMode on STM32L4+ series?
Thanks.
Solved! Go to Solution.
2018-09-07 9:07 AM
Ok the problem is resolved.
I used inside the interrupt the RTOS message queue and after the reset it was not initialized.
Sometimes it worked, sometimes not, funny.
Sorry for that!
2018-09-07 9:07 AM
Ok the problem is resolved.
I used inside the interrupt the RTOS message queue and after the reset it was not initialized.
Sometimes it worked, sometimes not, funny.
Sorry for that!