Question
STM32L476RG Nucleo: Failed to load flash loader IAR 7.3 EWARM 7.5
Posted on February 29, 2016 at 17:39
Running the most up to date EWARM on IAR. I receive the following problem in my Debug Log:
Mon Feb 29, 2016 10:17:59: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.3\arm\config\debugger\ST\STM32L4xx.dmac Mon Feb 29, 2016 10:17:59: Loaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.3\arm\config\flashloader\ST\FlashSTM32L4xxx.mac Mon Feb 29, 2016 10:17:59: Connected to ST-Link/V2-1 [SWD mode 1800 kHz] Firmware V2.J23.S6 (Probe no: 74622707) Mon Feb 29, 2016 10:17:59: Software reset was performed Mon Feb 29, 2016 10:17:59: Initial reset was performed Mon Feb 29, 2016 10:17:59: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.3\arm\config\flashloader\ST\FlashSTM32L4xxx.mac(13,33): Error: Operation error. Mon Feb 29, 2016 10:17:59: Error while calling macro execUserFlashInit Mon Feb 29, 2016 10:17:59: Unloaded macro file: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.3\arm\config\flashloader\ST\FlashSTM32L4xxx.mac Mon Feb 29, 2016 10:17:59: Failed to load flash loader: C:\Program Files (x86)\IAR Systems\Embedded Workbench 7.3\arm\config\flashloader\ST\FlashSTM32L4xxxG.flash I made sure to check to make sure my ST Link utilities were up to date and have selected SBW in my project options under ST link. I also made sure my device firmware was upd to date and can talk to the board. Using IAR 7.3.4, EWARM 7.50.3Please help!