Skip to main content
Geoffrey1
Senior
Mar 27, 2018 1:36 PM UTC
Solved

stm32l432 boot sequence (specifically from previously empty flash)

Posted on March 27, 2018 at 15:36

The stm32l432 reference manual has the following cryptic remark about the boot sequence

'A Flash empty check mechanism is implemented to force the boot from system Flash if the first Flash memory location is not programmed (0xFFFF FFFF) and if the boot selection was configured to boot from the main Flash.'

But does not specify when this check occurs.  I've found the following anomaly that may relate to this.  

1) Start with an erased device

2) Program the part

3) Without power cycling, reset

In this case, the part will jump to the system boot loader.  However, the mysterious thing is that  SYSCFG->MEMRMP is 0 (indicating that the memory is not remapped).   I don't see how it is possible to boot to the programmed code without a power cycle -- even through the SWD interface, because it appears that the 'Flash empty check' is persistent.   What am I missing ?    I know how to use the SWD interface to access all of the stm32 resources, but I don't see what visible state is affecting the boot sequence.

    This topic has been closed for replies.
    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    Aug 19, 2018 12:45 PM UTC

    Ok, if NVIC_SystemReset() isn't sufficient, what about a transition through STANDBY?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

    8 replies

    MSonn
    Visitor II
    Aug 9, 2018 3:05 PM UTC

    Hi Nickname6476,

    We seem to have the same issue with STM32L496.

    We program a new device (which has its flash empty). Then, in order for it to boot from flash we must power-cycle it (or otherwise it seems to keep booting into bootloader)

    Do you happen to have some more info please?

    Thanks,

    Moti

    Geoffrey1
    Geoffrey1Author
    Senior
    Aug 19, 2018 12:23 PM UTC

    I don't have any further information. Actually, this worries me a bit since I'm building very small devices with soldered on batteries. While I have a process that can handle the initial case -- program the parts before adding the battery -- I'm concerned about what happens if I reprogram the parts and get into this state.

    Tesla DeLorean
    Tesla DeLoreanBest answer
    Guru
    Aug 19, 2018 12:45 PM UTC

    Ok, if NVIC_SystemReset() isn't sufficient, what about a transition through STANDBY?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Geoffrey1
    Geoffrey1Author
    Senior
    Aug 27, 2018 10:59 AM UTC

    Ok, it's super irritating that nobody from ST has weighed in on what is clearly an issue with the STM32L4. I appreciate Clive's suggestion, but really don't want to try random things requiring a lot of work. I want a clear explanation of what the bootloader hardware support is doing, why, and how to flash and reset a battery powered device when disconnecting power is infeasible.

    Geoffrey1
    Geoffrey1Author
    Senior
    Aug 27, 2018 11:46 AM UTC

    ok, I haven't tried this yet. The following note in the reference manual about the flash status register FLASH_SR:

    Set by hardware on power-on reset or after OBL_LAUNCH command execution

    if the Flash is not programmed and the user intends to boot from the main Flash.

    Cleared by hardware on power-on reset or after OBL_LAUNCH command

    execution if the Flash is programmed and the user intends to boot from main

    Flash. This bit can also be set and cleared by software.

    1: The bit value is toggling

    0: No effect

    This bit can be set to clear the Program Empty bit if an OBL_LAUNCH is done by

    software after Flash programming (boot in main flash selected). It finally forces

    the boot in the main flash, without loosing the debugger connection.

    So it looks like (still need to test) that after a flashing a blank memory, it's necessary to either do a power cycle or set the OBL_LAUNCH bit in the FLASH_CR

    Tesla DeLorean
    Guru
    Aug 27, 2018 12:57 PM UTC

    It is Europe, I assume everyone disappears through August.. Poke your local FAE

    Not sure it was random, bit of a cheap shot perhaps, but based on some sound reasoning/logic, and the assumption you're were not using a plutonium battery, and the device would being going into STANDBY in the nature order of things to have some discernible battery life.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Geoffrey1
    Geoffrey1Author
    Senior
    Aug 27, 2018 2:17 PM UTC

    Perhaps a cheap shot -- my apologies. But, getting to shutdown from the debugger interface is a bit harder than from code since it requires injecting some code and then executing it. I did try out OBL_LAUNCH above without success (even after unlocking the flash). I'm looking for a solution that can easily be performed through the debugger.

    Geoffrey1
    Geoffrey1Author
    Senior
    Aug 28, 2018 1:45 PM UTC

    I didn't like going through gdb. Here's an openocd routine that will do the job :

    proc clear_erase () {

      reset halt

      puts [reg 15]

      step

      mdw 0x40022014 1

      # unlock flash                                

      mww 0x40022008 0x45670123

      mww 0x40022008 0xCDEF89AB

      mdw 0x40022014 1

      # unlock option                               

      mww 0x4002200c 0x08192A3B

      mww 0x4002200c 0x4C5D6E7F

      mdw 0x40022014 1

      # lauch option byte loader                          

      puts "launch option byte loader"

      mww 0x40022014 0x08000000

    }

    Here's a gdb script that seems to do the trick -- it connects to the serve (openocd), loads the binary and steps into the reset vector, unlocks the flash, write the flash CR, steps, and exits. Along the way it prints the contents of the flash CR serveral times.

    target ext :3333

    load

    step

    p/x *0x40022014

    set *0x40022008=0x45670123 

    set *0x40022008=0xCDEF89AB

    p/x *0x40022014

    set *0x40022014=0x08000000

    step

    p/x *0x40022014

    c