cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L4 usb_mic clock config

Posted on June 15, 2018 at 11:45

hello,

I'm trying to implement a USB microphone using STM32L4 discovery board.

I have started with the USB device example and now trying to add the microphone.

The library have given us the stm32l476g_discovery_audio.c

with the following functions

- BSP_AUDIO_IN_Init(SAI_AUDIO_FREQUENCY_48K,16,1)

- BSP_AUDIO_IN_Record(RecBuff,2048);

both returned AUDIO_OK but nothing is written to the 

RecBuff.. Is there a know problem with these fuctions?

socondly, how can we add USB clock config to the PeriphClockSelection?

The given code in 

stm32l476g_discovery_audio.c in AUDIO_SAIPLLConfig does the following

// SAI clock config//

//PLLSAI1_VCO= 8 Mhz * PLLSAI1N = 8 * 43 = VCO_344M//

//SAI_CK_x = PLLSAI1_VCO/PLLSAI1P = 344/7 = 49.142 Mhz //

RCC_ExCLKInitStruct.PeriphClockSelection = RCC_PERIPHCLK_SAI1;

RCC_ExCLKInitStruct.PLLSAI1.PLLSAI1N = 43;

RCC_ExCLKInitStruct.PLLSAI1.PLLSAI1P = 7;

RCC_ExCLKInitStruct.PLLSAI1.PLLSAI1ClockOut = RCC_PLLSAI1_SAI1CLK;

I have tried this, not sure if it's a proper solution

RCC_ExCLKInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USB | RCC_PERIPHCLK_SAI1;

RCC_ExCLKInitStruct.PLLSAI1.PLLSAI1N = 43;

RCC_ExCLKInitStruct.PLLSAI1.PLLSAI1P = 7;

RCC_ExCLKInitStruct.PLLSAI1.PLLSAI1ClockOut = RCC_PLLSAI1_SAI1CLK;

RCC_ExCLKInitStruct.Sai1ClockSelection = RCC_SAI1CLKSOURCE_PLLSAI1;

RCC_ExCLKInitStruct.UsbClockSelection = RCC_USBCLKSOURCE_MSI;
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0