cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L - Programming issue -> Internal command error

Avan .9
Associate

I cannot program the STM32L with the STM32 ST-Link Ultility (hex file).

Did reseach on internet and I know there is a lot on this subject already!

The setup is easy, I have a replica ST-linkv2 from China and an official Stlink v3 programmer.

I'm programming with SWDIO, GND and SWCLK with external power without any problems.

Also I have an official St-link v2 and the st-link v2-isol and there is my problem (new ones).

The same setup, just three pins with external power and I cannot program my board.

The first thing here are, checking the pins and update the firmware of the programmer.

So for both st-links I use pin 7 SWDIO, p20 as GND and p9 for SWCLK as described from the datasheet (Table 3 SWD cable connections - from top view). No luck here.

Did a firmware upgrade from the latest software without luck and even did it again from the seperate tool on the website "stsw-link007.zip".

Progam details are straight forward.

  • Connection settings: SWD with frequency 4.0 MHz (did tried it on 1.8 -> no luck).
  • Mode: Normal with low power enable
  • Reset Mode: Software System Reset

I can see the chip with Mode: "Hot Plug" device ID etc but cannot program it.

All no luck and if I use the v3 or the replica programmer it all works directly.

I should forget something but I do not know what..

Thank you for your time!

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Avan .9
Associate

Edit: I updated to the latest drivers as well from the this website.