cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H523HEYX flash write issue

yb25Kim
Visitor

STM32H523HEYX Flash Write Issue

1.
I’m currently working on a project using the STM32H523HEYX.
I'm using STM32CubeIDE, and the firmware libraries are up to date.
I’m also using STM32 X-CUBE-FREERTOS.

I’m trying to write data to Flash memory using the following functions:


2. HAL_FLASHEx_Erase(...);
HAL_FLASH_Program(FLASH_TYPEPROGRAM_QUADWORD, ASDF, (uint32_t)&quadData[0]);
However, the code triggers a HardFault when executed.

3. When I run the same code on a STM32H533 Nucleo board, it works without any fault and writes to Flash successfully.

4. I'm not sure why this Flash issue only occurs on the STM32H523HEYX.
If anyone has experienced a similar issue or knows of any related problems, I’d appreciate your advice.

Thank you, fellow developers!

0 REPLIES 0