cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G070RB8TX- Board Malfunctioning

SBHAR.16
Associate

I am using STMG32G070RB8TX for Programming the device is detected in TS link Utility but when i compile the compiler throws an error below is the description of the error.

Error in final launch sequence:

Error in initializing ST-LINK device.

Reason: (255) Unknown. Please check power and cabling to target.

Error in initializing ST-LINK device.

Reason: Unknown. Please check power and cabling to target.

Starting server with the following options:

    Persistent Mode      : Disabled

    Logging Level       : 1

    Listen Port Number     : 61234

    Status Refresh Delay    : 15s

    Verbose Mode        : Disabled

    SWD Debug         : Enabled

Target unknown error 19

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0