2018-08-19 9:13 PM
STM32F765 not supported in IAR workbench. (version 7.40)
so i can not load example project in stm32cubef7.
there is no "STM32F765" in device list in project setting menu
do I need to upgrade IAR workbench version? or any other way?
nordic semi mcu, Nordic supplied latest mcu MDK file to support IAR workbench.
does ST has same package?
2018-08-20 4:38 AM
Tried IAR support?
Might have to move to V8, or pick a part which is a close match and modify the ICF.
See if processor list is XML or something you can self modify.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.