cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f746x SPI strange data size

jvankuilenburg
Associate II
Posted on November 12, 2015 at 13:47

I have a problem with the datasize of the SPI of the stm32f746.

When I set the size (DS in CR2) 0111: 8-bit or lower, the spi gives double clock pulses. When I set the size 1000: 9-bit or bigger, the clock pulses are equivalent with the setting of the data size. What should be the problem?

The settings are (controlled by reading the regs) :

CR1: 0x0074

CR2: 0x1704

I2SCFGR : 0x0000

uint8_t spi_8send(SPI_TypeDef* SPIx, uint8_t data)

{

   SPIx->DR = data; // write data to be transmitted to the SPI data register

   

   while(1);

blocked, for debugging with the scope, then I see 16 clock pulses

   

   while( !(SPIx->SR & SPI_I2S_FLAG_TXE) || (SPIx->SR &SPI_FIFO_FTLVL)); // wait until transmit complete

   while( !(SPIx->SR & SPI_I2S_FLAG_RXNE) ); // wait until receive complete

   while( SPIx->SR & SPI_I2S_FLAG_BSY ); // wait until SPI is not busy anymore

   return SPIx->DR; // return received data from SPI data register

}

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
stm322399
Senior
Posted on November 12, 2015 at 14:03

According RM0385 chapter 32.5.8 Data transmission and reception, when the size is 8-bit or less, two characters are packed into the 16-bit DR. Using SPIx->DR writes the whole 16-bit, resulting in (almost) the same effect as two 8-bit accesses.

jvankuilenburg
Associate II
Posted on November 26, 2015 at 11:26

Thanks!

It's solved:

uint8_t spi_8send(SPI_TypeDef* SPIx, uint8_t data)

{

   *((volatile uint8_t*)&SPIx->DR) = data; // write data to be transmitted to the SPI data register

   while( !(SPIx->SR & SPI_I2S_FLAG_TXE) || (SPIx->SR & SPI_FIFO_FTLVL))  _spi_printstatus(SPIx); // wait until transmit complete

   while( !(SPIx->SR & SPI_I2S_FLAG_RXNE) )  _spi_printstatus(SPIx); // wait until receive complete

   while( SPIx->SR & SPI_I2S_FLAG_BSY )  _spi_printstatus(SPIx); // wait until SPI is not busy anymore

   return SPIx->DR; // return received data from SPI data register

}