cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F722IEK6 processor not counting properly

Brian D
Associate III
Posted on April 21, 2018 at 02:41

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This discussion is locked. Please start a new topic to ask your question.
13 REPLIES 13
Posted on April 22, 2018 at 00:41

Hi Joerg, I just installed Eclipse IDE package recently and so it is currently set to default. But I will look for the effects of instruction catch enabled.

.

Brian D
Associate III
Posted on April 23, 2018 at 22:43

This problem appeared with the chip ran under debug mode, and so today I thought might be it would be fine if I flash the chip with release configuration. After generated the .elf in the release folder, I went to target > program chip > but the tool does not provide the option to choose the release folder; only the debug folder is available. My co-worker has both the release and debug folders under target > program chip. Anyone know why I don't have the release folder?

Posted on April 23, 2018 at 22:53

You'll need to get familiar with the tool chain you have chosen and the multitude of settings in configuration, installation and metadata, that control what, where and how things are built.

If the project description file is in XML I suppose you could use a diff or merge tools to observe the differences between the two system.

Keil has option tabs controlling what directories output is directed too.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Brian D
Associate III
Posted on April 24, 2018 at 03:34

OK, I think here is the reason why the for() loop counter is so unpredictable. It seems the compiler might optimize or ignore a dummy loop as the for(n=0; n< 500; n++); 

So I changed it to

for(n=0; n<100; n++)    Temp = SPI2.DR;      // read SPI2 data register (assuming 100X read would have the same delay as wished. This forced the tool not to ignore or did funny thing with the loop, and I got the consistence counting delay.

So the lesson learned is do not use an empty for() loop for delay -- it is unreliable. 

Thank you all for trying to help.