cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F7 Discovery Demo in Eclipse

l239955_stm1
Associate II
Posted on March 14, 2016 at 15:48

Hello there,

I´m testing STM32F7 Discovery board, is somewhere demonstration example for Eclipse (openstm) or only for IAR?

 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee
Posted on March 14, 2016 at 17:44

Hi paroulek.lukas,

The 

http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1897/PF261909

 package contains several examples configured for IAR, Keil and SW4STM32.

The demonstration example with SW4STM32 is available in STM32Cube_FW_F7_V1.3.0\Projects\STM32746G-Discovery\Demonstration\SW4STM32.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.