cancel
Showing results for 
Search instead for 
Did you mean: 

[STM32F7 Discovery] - BSP Libraries

federicoanoto
Associate II
Posted on October 30, 2015 at 20:15

Hello, can someone please tell me  how to add succesfully BSP drivers after generating a project on Keil with STM32CUBEMX.

Thanks.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Nesrine M_O
Lead II
Posted on November 02, 2015 at 10:17

Hi noto,

“how to add succesfully BSP drivers after generating a project on Keil with STM32CUBEMX�

BSP drivers are integrated manually in the project, I don’t know which kind of problem you are facing when adding drivers.

I propose that you have a look to the BSP example under STM32Cube F7 package and try to compare the project settings (include Paths, Define) with yours as first step.

STM32Cube_FW_F7_V1.2.0\Projects\STM32746G-Discovery\Examples\BSP\MDK-ARM

-Syrine-