2015-10-06 12:10 PM
Hi.
I've started to play with STM32F7 discovery. I got to DSP audio example from hands-on and I would like to use line-in instead of microphones. Unfortunately when I've changedBSP_AUDIO_IN_OUT_Init(INPUT_DEVICE_DIGITAL_MICROPHONE_2, OUTPUT_DEVICE_HEADPHONE, 90, DEFAULT_AUDIO_IN_FREQ); to
BSP_AUDIO_IN_OUT_Init(INPUT_DEVICE_INPUT_LINE_1, OUTPUT_DEVICE_HEADPHONE, 90, DEFAULT_AUDIO_IN_FREQ);
Only thing that's coming is noise. Could anyone help me to get line-in working?
Best regards
Konrad
#https://github.com/laurent-lator #stm32f7-audio
2016-01-30 6:48 AM
I can't believe it's that simple :)
Thank you.2016-01-30 12:15 PM
You can try this hex file.
________________ Attachments : Line_in_2_phones.hex : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hzid&d=%2Fa%2F0X0000000bOh%2F8i4ra6h9VbGhL8kkfHfdUEAr04UF5HBm5_IqxV5FNn4&asPdf=false2016-02-18 2:25 PM
Yes, volume < 70!
I made same experience. And, if I remember correctly: the ADC/DAC chip is configured with an audio cross connect (inside the onboard ADC/DAC chip, this WM9... chip). I have modified slightly the config for this chip (done via very low level driver code, via I2C) and it works fine for me. I think, this DAC chip has feedback or taken some audio from another channel/input and volume > 70 results in just distortions (noise) due to active audio cross/feedback.2016-10-07 8:50 AM
Hi David.
I managed to build your program with System Workbench. Have you found out what causes the noise yet? The noise level is just totally ridiciolus. Totally useless in its current configuration.2018-07-25 4:20 AM
Hello Nickname8353,
Can you tell me from where can I finde DSP example code for STM32F7 Discovery? I am trying to generate audio signal from audio out. and also taking input from audio line in and same signal to audio out. It will be great helpfull.
Thank You.