STM32F437 USB VBUS sensing intermittently fails to detect disconnection
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-03-08 2:45 PM
Posted on March 08, 2017 at 23:45
We have a device which is self powered USB peripheral, using the ST provided USB stack, I'm seeing the device fail to detect the loss of VBUS (notified via the SEDET interrupt). It works approximately 70% of the time. The voltage on VBUS is going to 0 so it's not a pull up issue.
Is there a way to read the state of VBUS? I'm wondering if it's a software bug and the interrupt bit is being incorrectly cleared without being handled, but I couldn't find anywhere where I could read the current state of the VBUS detection? I guess the other option is to poll this line as a GPIO, but this seems like a hack.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0