cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429IG - USB FS Device mass storage + SDIO - not working

198031
Associate
Posted on December 06, 2014 at 19:13

Hello,

I want use USB + SD SDIO. I used standard libraries from ST but I still get following messages:

> MSC Interface started. 

USB Device Library v1.1.0 [FS] 

USB Device Library v1.1.0 [FS] 

> MSC Interface started. 

USB Device Library v1.1.0 [FS] 

USB Device Library v1.1.0 [FS] 

> MSC Interface started. 

USB Device Library v1.1.0 [FS] 

USB Device Library v1.1.0 [FS] 

> MSC Interface started.

Does anyone have an idea how to solve this problem?
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on December 06, 2014 at 22:59

Does anyone have an idea how to solve this problem?

With the information provided, not so much.

The STM32F429I-DISCO has some pin conflicts on the SDIO interface, and seem to recall it using the HS interface. But who knows what board you're using.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
198031
Associate
Posted on December 06, 2014 at 23:45

I'm using this board: http://www.wvshare.com/product/Open429I-C-Standard.htm

Posted on December 07, 2014 at 00:28

Ok, well I'm pretty sure none of ST's code targets this board. So you'll need to port any pin and board specific differences. This will require you review the schematics for both boards.

One of the more obvious ones would be that it uses an 8 MHz crystal, and all of ST's EVAL series boards use 25 MHz. So you'll have to address the PLL and HSE_VALUE settings.

The SDIO interface has an arbitrary GPIO used for CARD DETECT

Would recommend you try to confirm the SDIO interface is functional first.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..