cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F411 - Not getting lowest current consumption when putting device into standby

bm
Associate II
Posted on December 21, 2016 at 17:23

So I want my device to go into standby mode to run on the lowest power mode possible. Unfortunately, when measuring the current it does not drop below 360�A and I have no clue why...

This is my HSI setup:

configure_system_clock(void)

{

RCC_OscInitTypeDef RCC_OscInitStruct;

RCC_ClkInitTypeDef RCC_ClkInitStruct;

RCC_PeriphCLKInitTypeDef PeriphClkInitStruct;

__HAL_RCC_PWR_CLK_ENABLE();

__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;

RCC_OscInitStruct.HSIState = RCC_HSI_ON;

RCC_OscInitStruct.HSICalibrationValue = 16;

RCC_OscInitStruct.LSIState = RCC_LSI_OFF;

RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;

RCC_OscInitStruct.PLL.PLLM = 8;

RCC_OscInitStruct.PLL.PLLN = 192;

RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;

RCC_OscInitStruct.PLL.PLLQ = 8;

HAL_RCC_OscConfig(&RCC_OscInitStruct);

RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;

RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3);

return;

This is my main routine:

void main() {

HAL_SuspendTick();

volatile uint32_t x;

for (int i = 0; i < 599999; i++) {

for (int y = 0; y < 9; y++) {

volatile uint32_t x = +y;

}

}

__HAL_RCC_PWR_CLK_ENABLE();

__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);

HAL_PWR_EnableBkUpAccess();

__HAL_RCC_BACKUPRESET_FORCE();

__HAL_RCC_BACKUPRESET_RELEASE();

HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN1);

__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU);

HAL_PWR_EnterSTANDBYMode();

while(1);

}

No wakeup source configure since I just want to test standby current consumption.

Any idea what I am missing?

Thanks in advance.

#low-power-standby
This discussion is locked. Please start a new topic to ask your question.
19 REPLIES 19
Posted on December 21, 2016 at 18:22

1. We use a custom PCB but I'll try to find a discovery board. I'll use the same code and see if it behaves the same..

2. Well there is not much to explain. I want to put our device into standby mode to measure the current consumption. Therefore, we disconnected all external ICs, Oscillators, etc.. hooked up a battery and a power monitor. Regarding the code I had a look at the PWR_CurrentConsumption example in the cube package under STM32F411E-Discovery. The measured current consumption is 380µA. Too much for standby mode.

Posted on December 21, 2016 at 18:30

Hi

Moll.Benjamin

‌,

-Nesrine-

Posted on December 21, 2016 at 18:33

I will do this and let you know, thx!

Posted on December 22, 2016 at 13:47

It worked on the F411 Discovery board but not on my PCB. I guess I need to double check what draws the additional power :\

But thx anyways.

Posted on December 22, 2016 at 13:48

oh man; it worked on the F411 Discovery board but not on my PCB. I guess I need to double check what draws the additional power in my design :\

Bertrand DENIS
ST Employee
Posted on December 23, 2016 at 09:29

When the STM32F4 go into stand-by mode all the IOs are set into High impedance state. So I don't know if you measure the total power consumption of your board but you have to take it into account. Example : one IO driving an external input which will float, etc...

Please note that on STM32L4 you can program each state of IO in standby mode.

Posted on December 23, 2016 at 11:12

I am measuring the 3,3 line directly before the ST controller. We did a complete strip down of the PCB and removed everything; even the external OSC. Most of the I/O lines now are of course not routed. So no I/O can possibly drive another IC. 

strange...

Posted on December 23, 2016 at 15:13

Hi binaryguy,

be sure to configure all unused I/Os to either analog mode or output push-pull low.

Posted on December 23, 2016 at 15:43

So the 330µA could be traced back to a resistor that should not be present at all.

It's working now. Thank you!

But can someone finally confirm if I need to set my I/Os to analog-in before entering standby or not because in the HAL example code it is not done for standby but only for STOP mode.

Posted on December 23, 2016 at 21:36

You don't need because as written above all IOs are automatically set in high impedance when you enter in standby mode.