cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F401RE-Nucleo LED and BUTTON's problem

gpt1_account
Associate
Posted on April 07, 2015 at 18:27

Hi, 
 I am trying to run a simple program on my new Nucleo board,
 I made this program in order to turn on and off the green led when i press the user's button (the blue one),
 #include ''stm32f4xx.h''
#include ''stm32f4xx_nucleo.h''
#include ''system_stm32f4xx.h''
#include ''stm32f4xx_hal_gpio.h''
#include ''stm32f4xx_hal_rcc.h''
GPIO_InitTypeDef GPIO_InitStructure; 
int
main(
void
) {
HAL_Init(); 
__GPIOA_CLK_ENABLE();
GPIO_InitStructure.Pin = GPIO_PIN_5;
GPIO_InitStructure.Mode = GPIO_MODE_OUTPUT_PP; 
GPIO_InitStructure.Pull = GPIO_PULLUP;
GPIO_InitStructure.Speed = GPIO_SPEED_HIGH; 
HAL_GPIO_Init(GPIOA, &GPIO_InitStructure); 
__GPIOC_CLK_ENABLE();
GPIO_InitStructure.Pin = GPIO_PIN_13;
GPIO_InitStructure.Mode = GPIO_MODE_INPUT;
GPIO_InitStructure.Pull = GPIO_PULLDOWN;
GPIO_InitStructure.Speed = GPIO_SPEED_FAST;
HAL_GPIO_Init(GPIOC, &GPIO_InitStructure);
while
(1) {
if
(HAL_GPIO_ReadPin(GPIOC, GPIO_PIN_13)) { 
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_RESET); 
} 
else
{
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5, GPIO_PIN_SET);
}
}
}
 But i am getting wrong result:
 - when i press the user's button, nothing happen,
 - when i keep pressing the user's button and i restart (by pressing the black button), i get good result,
 It seems like the program checks the state of the blue button only at the first run, i don't know why,
 Please help me if you have any ideas of what the problem comes from, or if you have a running program that switch the led on button press.
 Thank you, 

#stm32f401re
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
l239955_stm1
Associate II
Posted on April 08, 2015 at 07:19

Hi samy,

do you have system clock configuration in your program?