Question
STM32F4 USART PROBLEM
Posted on October 02, 2015 at 23:18
Hi guys, I have a problem. I have a USB-RS232 converter and i'll do usart tutorial with STM32F4. Codes are working, but meaningless character viewing at the serial Hyper terminal program.
Baudrate 9600. Clock Configuration: HSE_VALUE=8000000 and PLL_M=8 as defined. But don't working. There are still meaningless characters.my problem is here :
http://s23.postimg.org/mbz2h0xm3/2015_10_03_00_05_57_Ekran_g_r_nt_s.png
I would be glad if you can help..My code is here:/*USART2 example, with IRQI am using a CP2102 USB-to-USART converter.Wiring connections: STM32F4 CP2102 PA2 (USART2 Tx) -> Rx PA3 (USART2 Rx) -> Tx*/#include <stdio.h>#include ''stm32f4xx.h'' char str[50];volatile uint32_t msTicks; /* counts 1ms timeTicks */void SysTick_Handler(void) { msTicks++;}// Delays number of Systicks (happens every 1 ms)static void Delay(__IO uint32_t dlyTicks){ uint32_t curTicks = msTicks; while ((msTicks - curTicks) < dlyTicks);}void setSysTick(){ // ---------- SysTick timer (1ms) -------- // if (SysTick_Config(SystemCoreClock / 1000)) { // Capture error while (1){}; }}void setup_Periph(){ GPIO_InitTypeDef GPIO_InitStructure; USART_InitTypeDef USART_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; // Enable the APB1 periph clock for USART2 RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE); // Enable the GPIOA clock, used by pins PA2, PA3 RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE); // Setup the GPIO pins for Tx and Rx GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOA, &GPIO_InitStructure); // Connect PA2 and PA3 with the USART2 Alternate Function GPIO_PinAFConfig(GPIOA, GPIO_PinSource2, GPIO_AF_USART2); GPIO_PinAFConfig(GPIOA, GPIO_PinSource3, GPIO_AF_USART2); USART_InitStructure.USART_BaudRate = 9600; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Tx | USART_Mode_Rx; USART_Init(USART2, &USART_InitStructure); /* Enable the USART2 receive interrupt and configure the interrupt controller to jump to USART2_IRQHandler() if the USART2 receive interrupt occurs */ USART_ITConfig(USART2, USART_IT_RXNE, ENABLE); NVIC_InitStructure.NVIC_IRQChannel = USART2_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); // Finally enable the USART2 peripheral USART_Cmd(USART2, ENABLE);}void USART_puts(USART_TypeDef *USARTx, volatile char *str){ while(*str){ // Wait for the TC (Transmission Complete) Flag to be set // while(!(USARTx->SR & 0x040)); while(USART_GetFlagStatus(USART2, USART_FLAG_TC) == RESET); USART_SendData(USARTx, *str); *str++; }}int main(void) { setSysTick(); setup_Periph(); sprintf(str,''MAHMUT''); USART_puts(USART2, str); while(1){ // Nothing done here since we are using interrupts } return 0;}