cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 UART programming

jernej
Associate
Posted on July 30, 2013 at 10:08

I have managed to make Flash loader demonstrator work with my FTDI.

 Whenever I want to connect to my STM32F4 Discovery board I have to do that in two steps. Firstly I connect proper pins from FTDI to PCB, then I open Flash loader demonstrator, chose my options and click next. Then I get this warning screen: No response from the target.

If i close this screen and then again click next I come to flash status page. This is really annoys me, becouse I get this window and I have to make a couple more clicks. Is there any solution to this problem, becouse if I want to programm 50 boards, that would take a lot more time.

#stm32f4-uart-programming-isp #stm32f4-uart
This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
Tomas DRESLER
Senior II
Posted on July 31, 2013 at 17:59

Use command-line mode of FLD.

Edison
fero182
Associate II
Posted on March 03, 2014 at 13:58

Hi, can someone help me? I need to modify this code to STM32F4 kit. Alternatively, I would need an example of the UART Bluetooth communications (HC-06) module STM32F4. Thanks for all the help :)

#include ''stm32f10x_usart.h''

#include ''stm32f10x_rcc.h''

#include ''stm32f10x_gpio.h''

#include ''misc.h''

int i;

//ErrorStatus HSEStartUpStatus;

void NVIC_Configuration(void);

void GPIO_Configuration(void);

void USART_Configuration(void);

void USART1_IRQHandler(void);

void UARTSend(const unsigned char *pucBuffer, unsigned long ulCount);

int main(void)

{

usart_rxtx();

while(1)

{

}

}

/******************************************************************************/

/* STM32F10x Peripherals Interrupt Handlers */

/******************************************************************************/

/**

* @brief This function handles USARTx global interrupt request

* @param None

* @retval None

*/

void USART1_IRQHandler(void)

{

if ((USART1->SR & USART_FLAG_RXNE) != (u16)RESET)

{

i = USART_ReceiveData(USART1);

if(i == '1'){

GPIO_WriteBit(GPIOA,GPIO_Pin_8,Bit_SET); // Set '1' on PA8

UARTSend(''LED ON\r\n'',sizeof(''LED ON\r\n'')); // Send message to UART1

}

else if(i == '0'){

GPIO_WriteBit(GPIOA,GPIO_Pin_8,Bit_RESET); // Set '0' on PA8

UARTSend(''LED OFF\r\n'',sizeof(''LED OFF\r\n''));

}

}

}

void usart_rxtx(void)

{

const unsigned char welcome_str[] = '' Welcome to Bluetooth!\r\n'';

/* Enable USART1 and GPIOA clock */

RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1 | RCC_APB2Periph_GPIOA, ENABLE);

/* NVIC Configuration */

NVIC_Configuration();

/* Configure the GPIOs */

GPIO_Configuration();

/* Configure the USART1 */

USART_Configuration();

/* Enable the USART1 Receive interrupt: this interrupt is generated when the

USART1 receive data register is not empty */

USART_ITConfig(USART1, USART_IT_RXNE, ENABLE);

/* print welcome information */

UARTSend(welcome_str, sizeof(welcome_str));

}

/*******************************************************************************

* Function Name : GPIO_Configuration

* Description : Configures the different GPIO ports

*******************************************************************************/

void GPIO_Configuration(void)

{

GPIO_InitTypeDef GPIO_InitStructure;

/* Configure (PA.8) as output */

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;

GPIO_Init(GPIOA, &GPIO_InitStructure); // Save

/* Configure USART1 Tx (PA.09) as alternate function push-pull */

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

GPIO_Init(GPIOA, &GPIO_InitStructure);

/* Configure USART1 Rx (PA.10) as input floating */

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10;

GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;

GPIO_Init(GPIOA, &GPIO_InitStructure);

}

/*******************************************************************************

* Function Name : USART_Configuration

* Description : Configures the USART1

*******************************************************************************/

void USART_Configuration(void)

{

USART_InitTypeDef USART_InitStructure;

/* USART1 configuration ------------------------------------------------------*/

USART_InitStructure.USART_BaudRate = 9600; // Baud Rate

USART_InitStructure.USART_WordLength = USART_WordLength_8b;

USART_InitStructure.USART_StopBits = USART_StopBits_1;

USART_InitStructure.USART_Parity = USART_Parity_No;

USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

USART_Init(USART1, &USART_InitStructure);

/* Enable USART1 */

USART_Cmd(USART1, ENABLE);

}

/**

* @brief Configures the nested vectored interrupt controller.

* @param None

* @retval None

*/

void NVIC_Configuration(void)

{

NVIC_InitTypeDef NVIC_InitStructure;

/* Enable the USARTx Interrupt */

NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn;

NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

NVIC_Init(&NVIC_InitStructure);

}

/*******************************************************************************

* Function Name : UARTSend

* Description : Send a string to the UART.

* Input : - pucBuffer: buffers to be printed.

* : - ulCount : buffer's length

*******************************************************************************/

void UARTSend(const unsigned char *pucBuffer, unsigned long ulCount)

{

//

// Loop while there are more characters to send.

//

while(ulCount--)

{

USART_SendData(USART1, (uint16_t) *pucBuffer++);

/* Loop until the end of transmission */

while(USART_GetFlagStatus(USART1, USART_FLAG_TC) == RESET)

{

}

}

}
Posted on March 03, 2014 at 14:20

Would probably have been something to start a new topic with.

Be aware that PA9 is not usable for the USART1 on the STM32F4-Discovery board, review schematic.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
fero182
Associate II
Posted on March 03, 2014 at 14:47

Can you help with that? This code works on STM32F1 .. but I need it to work on STM32F4. I will be very grateful :)

Posted on March 03, 2014 at 15:51

I'm not going to modify the STM32F4-Discovery design for you, if you want to modify the circuit and remove components you will need to review and understand the schematic. Tip: There is a VERY large bulk capacitor attached to PA9.

// STM32 USART3 (Tx PB.10, Rx PB.11) STM32F4 Discovery - sourcer32@gmail.com
#include ''stm32f4_discovery.h''
/**************************************************************************************/
void RCC_Configuration(void)
{
/* --------------------------- System Clocks Configuration -----------------*/
/* USART3 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE);
/* GPIOB clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE);
}
/**************************************************************************************/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/*-------------------------- GPIO Configuration ----------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10 | GPIO_Pin_11;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOB, &GPIO_InitStructure);
/* Connect USART pins to AF */
GPIO_PinAFConfig(GPIOB, GPIO_PinSource10, GPIO_AF_USART3);
GPIO_PinAFConfig(GPIOB, GPIO_PinSource11, GPIO_AF_USART3);
}
/**************************************************************************************/
void USART3_Configuration(void)
{
USART_InitTypeDef USART_InitStructure;
/* USARTx configuration ------------------------------------------------------*/
/* USARTx configured as follow:
- BaudRate = 9600 baud
- Word Length = 8 Bits
- One Stop Bit
- No parity
- Hardware flow control disabled (RTS and CTS signals)
- Receive and transmit enabled
*/
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART3, &USART_InitStructure);
USART_Cmd(USART3, ENABLE);
}
/**************************************************************************************/
int main(void)
{
RCC_Configuration();
GPIO_Configuration();
USART3_Configuration();
while(1)
{
uint16_t Data;
while(USART_GetITStatus(USART3, USART_IT_RXNE) == RESET); // Wait for Char
Data = USART_ReceiveData(USART3); // Collect Char
while(USART_GetITStatus(USART3, USART_IT_TXE) == RESET); // Wait for Empty
USART_SendData(USART3, Data); // Echo Char
}
while(1); // Don't want to exit
}

// STM32 USART2 (Tx PD.5, Rx PD.6) STM32F4 Discovery - sourcer32@gmail.com
#include ''stm32f4_discovery.h''
/**************************************************************************************/
void RCC_Configuration(void)
{
/* --------------------------- System Clocks Configuration -----------------*/
/* USART2 clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);
/* GPIOD clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);
}
/**************************************************************************************/
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/*-------------------------- GPIO Configuration ----------------------------*/
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_5 | GPIO_Pin_6;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(GPIOD, &GPIO_InitStructure);
/* Connect USART pins to AF */
GPIO_PinAFConfig(GPIOD, GPIO_PinSource5, GPIO_AF_USART2); // USART2_TX
GPIO_PinAFConfig(GPIOD, GPIO_PinSource6, GPIO_AF_USART2); // USART2_RX
}
/**************************************************************************************/
void USART2_Configuration(void)
{
USART_InitTypeDef USART_InitStructure;
/* USARTx configuration ------------------------------------------------------*/
/* USARTx configured as follow:
- BaudRate = 115200 baud
- Word Length = 8 Bits
- One Stop Bit
- No parity
- Hardware flow control disabled (RTS and CTS signals)
- Receive and transmit enabled
*/
USART_InitStructure.USART_BaudRate = 115200;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART2, &USART_InitStructure);
USART_Cmd(USART2, ENABLE);
}
/**************************************************************************************/
int main(void)
{
RCC_Configuration();
GPIO_Configuration();
USART2_Configuration();
while(1)
{
while(USART_GetFlagStatus(USART2, USART_FLAG_TXE) == RESET); // Wait for Empty
USART_SendData(USART2, 0x49); // Send 'I'
}
while(1); // Don't want to exit
}

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
fero182
Associate II
Posted on March 03, 2014 at 17:12

Thank clive1, but the terminal I / O in both examples is blank. Which can be a problem?

frankmeyer9
Associate II
Posted on March 03, 2014 at 17:32

A scope and/or the debugger are useful tools to find out where your characters get stuck.

Posted on March 03, 2014 at 19:04

The STM32 outputs at CMOS levels, consider what you have connected it too, and the signals observed on a scope.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..