Skip to main content
jason22
Associate II
May 20, 2012
Question

STM32F4-Discovery with USB(CDC), LCD, Web Interface...

  • May 20, 2012
  • 3 replies
  • 876 views
Posted on May 20, 2012 at 03:55

I must say, the STM32F4-Discovery is most definitely the most accessible microcontroller I've ever worked with. I now have a fully working USB via CDC(ie. virtual com port), an LCD for basic data display, and now a Web-based(PHP) scripted-linked to a linux bash-script for interfacing(reading,writing) to the com port. Amazing what you can do with these things!

If anyone would like some help and/or guidance on the above, feel free to ask.

#compatible-!=-zero-effort #stm32f4-discovery-usb-cdc-web
    This topic has been closed for replies.

    3 replies

    bjfree
    Associate II
    May 20, 2012
    Posted on May 20, 2012 at 06:03

    add to that CAN interface, with a Wifi. SD storage for the pages.

    vikram2399
    Associate II
    May 21, 2012
    Posted on May 21, 2012 at 07:24

    Hi,

    I have bought STM32F4-discovery board.

    I have downloaded the firmware library version stm32f4discovery_fwV1.1.0 available on ST website.

    However this version does not contain  any codes for MSC or HID or UART application.

    It only has the IO_Toggle application project. That is working fine.

    Now I want to try and run the projects that were provided for STM32F2xx evaluation boards on the discovery board.

    But when I directly load the project on the discovery board nothing works though both F2 & F4  are compatible as per ST website.

    Can you please help me in this matter.

    Tesla DeLorean
    Guru
    May 21, 2012
    Posted on May 21, 2012 at 14:19

    But when I directly load the project on the discovery board nothing works though both F2 & F4  are compatible as per ST website.

    You were arguing this point last week, and while the physical parts are extremely similar (compatible to the point you can solder down one part instead of the other with a suitably thought out design), you will need to account for the differences in clock speeds, and wiring on the specific boards you want to use. You will need to do the code review and porting work yourself, if this does not appeal to you, you could hire one of the consultants/contractors that ST keeps a list of.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..