cancel
Showing results for 
Search instead for 
Did you mean: 

[STM32F4-Discovery] UART4 Problem

regiuliano2009
Associate II
Posted on February 24, 2012 at 12:36

Hi all,

I'm searching to get work my UART4 port on my Discovery. I used the USART HyperTerminal_Interrupt example on stdPerif_example and I adapted to DISCOVERY.

I see by some LedOn on the program that UART is working and sending interrupt.

I manage to have a virtual USB-UART port with UM232R Ftdi but on my Putty nothing appeared

I post my code

  /* USARTx configuration ------------------------------------------------------*/

  /* USARTx configured as follow:

        - BaudRate = 9600 baud

        - Word Length = 8 Bits

        - Two Stop Bit

        - Odd parity

        - Hardware flow control disabled (RTS and CTS signals)

        - Receive and transmit enabled

  */

  USART_InitStructure.USART_BaudRate = 9600;

  USART_InitStructure.USART_WordLength = USART_WordLength_8b;

  USART_InitStructure.USART_StopBits = USART_StopBits_2;

  USART_InitStructure.USART_Parity = USART_Parity_Odd;

  USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

   

  USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

  STM_EVAL_COMInit(&USART_InitStructure);

Function

void STM_EVAL_COMInit(USART_InitTypeDef* USART_InitStruct)

{

  GPIO_InitTypeDef GPIO_InitStructure;

  /* Enable GPIO clock */

  //RCC_AHB1PeriphClockCmd(UART4_TX_PIN | UART4_RX_PIN, ENABLE);

  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE); //clock a PORTC

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_UART4, ENABLE); //clock alla UART4!

  /* Connect PXx to USARTx_Tx*/

  GPIO_PinAFConfig(GPIOC, GPIO_Pin_10, GPIO_AF_UART4);

  /* Connect PXx to USARTx_Rx*/

  GPIO_PinAFConfig( GPIOC, GPIO_Pin_11, GPIO_AF_UART4);

  /* Configure USART Tx as alternate function  */

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

  GPIO_Init(GPIOC, &GPIO_InitStructure);

  /* Configure USART Rx as alternate function  */

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11;

  GPIO_Init(GPIOC, &GPIO_InitStructure);

  /* USART configuration */

  USART_Init(UART4, USART_InitStruct);

  /* Enable USART */

  USART_Cmd(UART4, ENABLE);

}

I also add

void UART4_IRQHandler(void); to _it.h to manage interrupt

_it.c

void UART4_IRQHandler(void)

{

    if(USART_GetITStatus(UART4, USART_IT_RXNE) != RESET)

  {

         GPIO_SetBits(GPIOD, GPIO_Pin_14); // accende led

    /* Read one byte from the receive data register */

    RxBuffer[RxCounter++] = (USART_ReceiveData(UART4) & 0x7F);

    if(RxCounter == NbrOfDataToRead)

    {

      /* Disable the UART4 Receive interrupt */

      USART_ITConfig(UART4, USART_IT_RXNE, DISABLE);

    }

  }

  if(USART_GetITStatus(UART4, USART_IT_TXE) != RESET)

  {

      GPIO_SetBits(GPIOD, GPIO_Pin_13); // accende led

      /* Write one byte to the transmit data register */

    USART_SendData(UART4, TxBuffer[TxCounter++]);

    if(TxCounter == NbrOfDataToTransfer)

    {

      /* Disable the UART4 Transmit interrupt */

      USART_ITConfig(UART4, USART_IT_TXE, DISABLE);

    }

  }

}

Where I'm failing?

THanks

#uart/usart-parity-and-wordlengt
This discussion is locked. Please start a new topic to ask your question.
40 REPLIES 40
jeannot
Associate II
Posted on May 12, 2015 at 16:29

hi,

i am new on this page but i need some help.

Please im working on STM32F4  and i want now to write an code with the microphono on board. I want to have finally an 16 bit on output of Pdm (PCM).

there is a way to do it?

thanks

giovani