2015-05-01 12:29 AM
Hi all,
I will configure HSE_VALUE = 8000000 and defined #define HSE_VALUE ((uint32_t)8000000) #define PLL_M 8 #define PLL_Q 7 #define PLL_N 336 #define PLL_P 2 And I defined line option : -DHSE_VALUE=8000000 My stm32f3-discovery connected to PC via (USB to COM) (FTDI - FT232) use UART4 and PIN PC10&PC11(TX & RX) and GND, but the Terminal on PC will received wrong ! How I passed this error?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.