Skip to main content
anuja
Associate II
May 27, 2014
Question

stm32f4 Discovery board UART DMA interrupt is not being serviced.

  • May 27, 2014
  • 4 replies
  • 939 views
Posted on May 28, 2014 at 00:02

Hi,

I'm trying to configure the UART in DMA mode, but I cannot get the interrupts to work.

I have attached my code.

Any help will be appreciated.

Thanks
    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    May 28, 2014
    Posted on May 28, 2014 at 02:55

    C++ with code/definitions missing

    Have the IRQHandler names gotten mangled? Check the .MAP file, check the linkage to the vector table. extern ''C'' ??

    // Clear DMA Transfer Complete interrupt pending bit. DMA_ClearITPendingBit(DMA1_Stream3, DMA_IT_TCIF1);

    DMA_IT_TCIF3?

    DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)mpoRxQueue; // Pointer to Reception Queue.

    Are you sure this is the buffer address and not the object?

    // Enable DMA Stream Half Transfer interrupt. DMA_ITConfig(DMA1_Stream1, DMA_IT_HT, ENABLE);

    You are not servicing the HT interrupt.

    If you still have problems, make sure that the DMA isn't signalling any errors.
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    anuja
    anujaAuthor
    Associate II
    May 28, 2014
    Posted on May 28, 2014 at 18:47

    Thanks Clive.

    I corrected the code to point to the correct bit.

    I was concentrating on the Tx code and had not looked into the Rx part. Thanks for debugging that it was pointing to an object instead of an array.

    I added the Interrupt for Transfer Error, none of the interrupts are getting triggered.

    The mapping in the vector table is correct. I have externed ''C'' the entire stm32f4xx_it.c file.

    I cannot figure out why the interrupts are not getting serviced. 

     

    waclawek.jan
    Super User
    May 29, 2014
    Posted on May 29, 2014 at 08:44

    Read out and post value of USART3 registers and the DMA registers of relevant streams' + LISR/HISR.

    JW

    anuja
    anujaAuthor
    Associate II
    May 29, 2014
    Posted on May 29, 2014 at 22:39

    Thanks for pointing me towards the registers Jan. 

    Turns out the register values were not getting updated because I had not set the RCC clock value correctly.