Skip to main content
roberto23
Associate
August 30, 2015
Question

STM32F4: Canbus bootloader

  • August 30, 2015
  • 1 reply
  • 656 views
Posted on August 30, 2015 at 17:10

Hello,

i see that if i activate the bootloader with BOOT0=1 and BOOT1=0 the system stay in the bootloader cycle all the time i mantain the pin configured in this way until restart the cpu.

Is possible to jump directly to the main user program if after a timeout no request is coming from outside to the cpu?

I'm asking because i have usually no access to the pcb when the final product is finished and i need to upload new program via bootloader. 

Thank you
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    August 30, 2015
    Posted on August 30, 2015 at 17:37

    If you want to control the behaviour you need to get your own loader on the chip earlier in the process.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..